Basler Vision Connector Messaging: Defining the Default Configuration
With the GenICam protocol you can store parameter sets on the camera, and with the Basler Vision Connector you can save, load, and define the default user set to be used on camera restart.
To determine the default camera parameter set, loaded to the camera during camera restart, you can send the SetDefaultUserSet message.
JSON Payload
| Field | Optional | Type | Description |
| TransactionID | Yes | String | Transaction identification |
| Action | No | String | Method called. Fixed value: SetDefaultUserSet |
| DeviceID | No | String | Device identification |
| UserSet | No | String/Integer (64-bit signed) | {Value} or {IntValue} of the User Set Object as defined in Retrieving Available User Sets |
{
"TransactionID": "1232116",
"Action": "SetDefaultUserSet",
"DeviceID": "548451887",
"UserSet": "UserSet2"
}
Response Object
| Field | Optional | Type | Description |
| TransactionID | Yes | String | Transaction identification |
| ReturnCode | No | Integer (32-bit unsigned) | Message code following Message Codes |
| Message | Yes | String | Response message |
{
"TransactionID": "1232116",
"ReturnCode": 0,
"Message": "Default userset defined."
}