Image ROI#
ROI is short for region of interest (formerly AOI = area of interest).
If an image ROI has been specified, the camera will only transmit pixel data from within that region. On most cameras, this increases the camera's maximum frame rate significantly.
The image ROI settings are independent from the auto function ROI settings.
Using the Feature#
Changing Position and Size of an Image ROI#
With the factory settings enabled, the camera is set to a default resolution. However, you can change the position and size as required.
To change the position and size of the image ROI:
- Make sure the camera is idle, i.e., not capturing images.
- If you are using an ace Classic/U/L camera, set the
CenterXandCenterYparameters tofalse. -
Use the following parameters to specify the size of the image ROI:
WidthHeight
-
Use the following parameters to specify the position of the image ROI:
OffsetXOffsetY
The origin of the image ROI is in the top left corner of the sensor array (column 0, row 0).
Example: Assume that you have specified the following settings:
Width= 16Height= 10OffsetX= 2OffsetY= 6
This creates the following image ROI:
Info
For area scan cameras:
- On most cameras, decreasing the size (especially the height) of the image ROI increases the camera's maximum frame rate significantly.
- If the Binning feature is enabled, the settings for the image ROI refer to the binned lines and columns and not to the physical lines in the sensor.
- On boA5120-230cc and boA5120-230cm cameras, the
OffsetYparameter is not available. The position of the image ROI is always centered in vertically. - On boA13440-17cm cameras, the position of the image ROI is always centered horizontally and vertically. If you change the width of the image ROI, the
OffsetXparameter value adapts automatically so that the image ROI stays centered horizontally. If you change the height of the image ROI, theOffsetYparameter value adapts automatically so that the image ROI stays centered vertically.
Both theOffsetXandOffsetYparameters are read-only.
Info
For line scan cameras:
- For line scan cameras having more than one sensor line, the following applies:
If you set the image ROI height to 1, the camera output on aquisition depends on the number of camera sensor lines:- Cameras with 2 sensor lines:
The camera will output the color channels as follows:
G in one line, R and B alternating in the other. - Cameras with 3 sensor lines:
The camera will output all three channels (R, G, and B) on acquisition.
For information about the number of sensor lines available in a camera model, see the General Specifications table in the corresponding camera topic.
- Cameras with 2 sensor lines:
- On all racer 2 cameras, the
OffsetYparameter is not available. - On racer 2 cameras with CXP interface, the
Heightparameter is automatically set to 1 and can't be changed. For these cameras, the single lines are transmitted to the frame grabber individually. The frame grabber then combines them into a frame. - On racer 2 S cameras with GigE or 5GigE interface, you can add several lines to build a frame. Use the
Heightparameter to define the height of the image ROI, i.e., the height of the resulting frame that is transmitted to the host computer.
Minimum number of lines per frame: 1
Depending on the host computer, a low frame height (i.e. < 10 lines) may increase the CPU load of the host computer significantly.
The maximum number of lines per frame depends on the camera model:- For r2L2048-29gc, r2L2048-58gm, r2L2048-62g5c, r2L2048-172g5m, r2L4096-29gm, and r2L4096-84g5m cameras: 12000
- For r2L4096-14gc and r2L4096-42g5c cameras: 10000
Info
For racer 2 S GigE cameras, you can use the Counter and Data Chunks features, in combination with the trigger settings, to specify which lines belong to a frame and which frames belong to the correct test object.
Guidelines#
When you are specifying an image ROI, follow these guidelines:
| Guideline | Example |
|---|---|
OffsetX + Width ≤ WidthMax | Camera with a 1920 x 1080 pixel sensor:OffsetX + Width ≤ 1920 |
OffsetY + Height ≤ HeightMax | Camera with a 1920 x 1080 pixel sensor:OffsetY + Height ≤ 1080 |
The WidthMax and HeightMax parameter values adapt to the current settings for Binning, Decimation, or Scaling (if available).
Specifics#
Image ROI Sizes#
| Camera Model | Minimum Width | Minimum Height |
|---|---|---|
| a2A640-240gmSWIR | 4 | 1 |
| a2A640-240umSWIR | 4 | 1 |
| a2A1280-80gmSWIR | 4 | 1 |
| a2A1280-125umSWIR | 4 | 1 |
| a2A1920-51gcBAS | 4 | 2 |
| a2A1920-51gcIP67 | 4 | 2 |
| a2A1920-51gcPRO | 4 | 2 |
| a2A1920-51gmBAS | 4 | 1 |
| a2A1920-51gmIP67 | 4 | 1 |
| a2A1920-51gmPRO | 4 | 1 |
| a2A1920-160ucBAS | 4 | 2 |
| a2A1920-160ucPRO | 4 | 2 |
| a2A1920-160umBAS | 4 | 1 |
| a2A1920-160umPRO | 4 | 1 |
| a2A1920-165g5cBAS | 4 | 2 |
| a2A1920-165g5mBAS | 4 | 1 |
| a2A2048-35gmSWIR | 4 | 1 |
| a2A2048-37gcBAS | 4 | 2 |
| a2A2048-37gcPRO | 4 | 2 |
| a2A2048-37gmBAS | 4 | 1 |
| a2A2048-37gmPRO | 4 | 1 |
| a2A2048-110umSWIR | 4 | 1 |
| a2A2048-114g5cBAS | 4 | 2 |
| a2A2048-114g5mBAS | 4 | 1 |
| a2A2048-114ucBAS | 4 | 2 |
| a2A2048-114ucPRO | 4 | 2 |
| a2A2048-114umBAS | 4 | 1 |
| a2A2048-114umPRO | 4 | 1 |
| a2A2048-173cmSWIR | 48 | 4 |
| a2A2440-98g5cBAS | 4 | 4 |
| a2A2440-98g5mBAS | 4 | 4 |
| a2A2448-23gcBAS | 4 | 2 |
| a2A2448-23gcIP67 | 4 | 2 |
| a2A2448-23gcPRO | 4 | 2 |
| a2A2448-23gmBAS | 4 | 1 |
| a2A2448-23gmIP67 | 4 | 1 |
| a2A2448-23gmPRO | 4 | 1 |
| a2A2448-75ucBAS | 4 | 2 |
| a2A2448-75ucPRO | 4 | 2 |
| a2A2448-75umBAS | 4 | 1 |
| a2A2448-75umPRO | 4 | 1 |
| a2A2448-105g5cBAS | 4 | 2 |
| a2A2448-105g5mBAS | 4 | 1 |
| a2A2448-120cc | 48 | 2 |
| a2A2448-120cm | 48 | 2 |
| a2A2448-210cc | 48 | 2 |
| a2A2448-210cm | 48 | 2 |
| a2A2560-20gmSWIR | 4 | 1 |
| a2A2560-70umSWIR | 4 | 1 |
| a2A2560-131cmSWIR | 48 | 4 |
| a2A2590-22gcBAS | 4 | 2 |
| a2A2590-22gcPRO | 4 | 2 |
| a2A2590-22gmBAS | 4 | 1 |
| a2A2590-22gmPRO | 4 | 1 |
| a2A2590-60ucBAS | 4 | 2 |
| a2A2590-60ucPRO | 4 | 2 |
| a2A2590-60umBAS | 4 | 1 |
| a2A2590-60umPRO | 4 | 1 |
| a2A2600-20gcBAS | 4 | 2 |
| a2A2600-20gcPRO | 4 | 2 |
| a2A2600-20gmBAS | 4 | 1 |
| a2A2600-20gmPRO | 4 | 1 |
| a2A2600-64ucBAS | 4 | 2 |
| a2A2600-64ucPRO | 4 | 2 |
| a2A2600-64umBAS | 4 | 1 |
| a2A2600-64umPRO | 4 | 1 |
| a2A2840-14gcBAS | 4 | 2 |
| a2A2840-14gcIP67 | 4 | 2 |
| a2A2840-14gcPRO | 4 | 2 |
| a2A2840-14gmBAS | 4 | 1 |
| a2A2840-14gmIP67 | 4 | 1 |
| a2A2840-14gmPRO | 4 | 1 |
| a2A2840-14gmUV | 4 | 1 |
| a2A2840-48ucBAS | 4 | 2 |
| a2A2840-48ucPRO | 4 | 2 |
| a2A2840-48umBAS | 4 | 1 |
| a2A2840-48umPRO | 4 | 1 |
| a2A2840-48umUV | 4 | 1 |
| a2A2840-67g5cBAS | 4 | 2 |
| a2A2840-67g5mBAS | 4 | 1 |
| a2A2840-67g5mUV | 4 | 1 |
| a2A2840-86cc | 48 | 2 |
| a2A2840-86cm | 48 | 2 |
| a2A3536-9gcBAS | 4 | 2 |
| a2A3536-9gcPRO | 4 | 2 |
| a2A3536-9gmBAS | 4 | 2 |
| a2A3536-9gmPRO | 4 | 2 |
| a2A3536-31ucBAS | 4 | 2 |
| a2A3536-31ucPRO | 4 | 2 |
| a2A3536-31umBAS | 4 | 2 |
| a2A3536-31umPRO | 4 | 2 |
| a2A3536-42g5cBAS | 4 | 4 |
| a2A3536-42g5mBAS | 4 | 4 |
| a2A3840-13gcBAS | 4 | 2 |
| a2A3840-13gcPRO | 4 | 2 |
| a2A3840-13gmBAS | 4 | 1 |
| a2A3840-13gmPRO | 4 | 1 |
| a2A3840-45ucBAS | 4 | 2 |
| a2A3840-45ucPRO | 4 | 2 |
| a2A3840-45umBAS | 4 | 1 |
| a2A3840-45umPRO | 4 | 1 |
| a2A4096-9gcBAS | 4 | 2 |
| a2A4096-9gcIP67 | 4 | 2 |
| a2A4096-9gcPRO | 4 | 2 |
| a2A4096-9gmBAS | 4 | 1 |
| a2A4096-9gmIP67 | 4 | 1 |
| a2A4096-9gmPRO | 4 | 1 |
| a2A4096-30ucBAS | 4 | 2 |
| a2A4096-30ucPRO | 4 | 2 |
| a2A4096-30umBAS | 4 | 1 |
| a2A4096-30umPRO | 4 | 1 |
| a2A4096-44g5cBAS | 4 | 2 |
| a2A4096-44g5mBAS | 4 | 1 |
| a2A4096-67cc | 48 | 2 |
| a2A4096-67cm | 48 | 2 |
| a2A4200-12gcBAS | 4 | 2 |
| a2A4200-12gcPRO | 4 | 2 |
| a2A4200-12gmBAS | 4 | 1 |
| a2A4200-12gmPRO | 4 | 1 |
| a2A4200-40ucBAS | 4 | 2 |
| a2A4200-40ucPRO | 4 | 2 |
| a2A4200-40umBAS | 4 | 1 |
| a2A4200-40umPRO | 4 | 1 |
| a2A4504-5gcBAS | 4 | 2 |
| a2A4504-5gcIP67 | 4 | 2 |
| a2A4504-5gcPRO | 4 | 2 |
| a2A4504-5gmBAS | 4 | 1 |
| a2A4504-5gmIP67 | 4 | 1 |
| a2A4504-5gmPRO | 4 | 1 |
| a2A4504-18ucBAS | 4 | 2 |
| a2A4504-18ucPRO | 4 | 2 |
| a2A4504-18umBAS | 4 | 1 |
| a2A4504-18umPRO | 4 | 1 |
| a2A4504-27g5cBAS | 4 | 2 |
| a2A4504-27g5mBAS | 4 | 1 |
| a2A4504-42cc | 48 | 2 |
| a2A4504-42cm | 48 | 2 |
| a2A4508-6gcBAS | 4 | 2 |
| a2A4508-6gcPRO | 4 | 2 |
| a2A4508-6gmBAS | 4 | 1 |
| a2A4508-6gmPRO | 4 | 1 |
| a2A4508-20ucBAS | 4 | 2 |
| a2A4508-20ucPRO | 4 | 2 |
| a2A4508-20umBAS | 4 | 1 |
| a2A4508-20umPRO | 4 | 1 |
| a2A5060-4gcBAS | 4 | 2 |
| a2A5060-4gmBAS | 4 | 1 |
| a2A5060-15ucBAS | 4 | 2 |
| a2A5060-15umBAS | 4 | 1 |
| a2A5060-21g5cBAS | 4 | 2 |
| a2A5060-21g5mBAS | 4 | 1 |
| a2A5060-35cc | 48 | 2 |
| a2A5060-35cm | 48 | 2 |
| a2A5320-7gcBAS | 4 | 2 |
| a2A5320-7gcIP67 | 4 | 2 |
| a2A5320-7gcPRO | 4 | 2 |
| a2A5320-7gmBAS | 4 | 1 |
| a2A5320-7gmPRO | 4 | 1 |
| a2A5320-7gmip67 | 4 | 1 |
| a2A5320-23ucBAS | 4 | 2 |
| a2A5320-23ucPRO | 4 | 2 |
| a2A5320-23umBAS | 4 | 1 |
| a2A5320-23umPRO | 4 | 1 |
| a2A5320-34g5cBAS | 4 | 2 |
| a2A5320-34g5mBAS | 4 | 1 |
| a2A5320-52cc | 48 | 2 |
| a2A5320-52cm | 48 | 2 |
| a2A5328-4gcBAS | 4 | 2 |
| a2A5328-4gcIP67 | 4 | 2 |
| a2A5328-4gcPRO | 4 | 2 |
| a2A5328-4gmBAS | 4 | 1 |
| a2A5328-4gmIP67 | 4 | 1 |
| a2A5328-4gmPRO | 4 | 1 |
| a2A5328-15ucBAS | 4 | 2 |
| a2A5328-15ucPRO | 4 | 2 |
| a2A5328-15umBAS | 4 | 1 |
| a2A5328-15umPRO | 4 | 1 |
| a2A5328-22g5cBAS | 4 | 2 |
| a2A5328-22g5mBAS | 4 | 1 |
| a2A5328-35cc | 48 | 2 |
| a2A5328-35cm | 48 | 2 |
| acA640-121gm | 1 | 1 |
| acA640-300gc | 16 | 2 |
| acA640-300gm | 16 | 1 |
| acA640-750uc | 16 | 2 |
| acA640-750um | 16 | 1 |
| acA720-290gc | 2 | 2 |
| acA720-290gm | 1 | 1 |
| acA720-520uc | 2 | 2 |
| acA720-520um | 1 | 1 |
| acA800-200gc | 16 | 2 |
| acA800-200gm | 16 | 1 |
| acA800-510uc | 16 | 2 |
| acA800-510um | 16 | 1 |
| acA1280-60gc | 2 | 2 |
| acA1280-60gm | 1 | 1 |
| acA1300-60gc | 2 | 2 |
| acA1300-60gm | 1 | 1 |
| acA1300-60gmNIR | 1 | 1 |
| acA1300-75gc | 16 | 2 |
| acA1300-75gm | 16 | 1 |
| acA1300-200uc | 16 | 2 |
| acA1300-200um | 16 | 1 |
| acA1440-73gc | 2 | 2 |
| acA1440-73gm | 1 | 1 |
| acA1440-220uc | 2 | 2 |
| acA1440-220um | 1 | 1 |
| acA1600-20gc | 2 | 2 |
| acA1600-20uc | 2 | 2 |
| acA1600-60gc | 2 | 2 |
| acA1600-60gm | 1 | 1 |
| acA1920-25gc | 64 | 64 |
| acA1920-25gm | 64 | 64 |
| acA1920-25uc | 64a | 64a |
| acA1920-25um | 64a | 64a |
| acA1920-40gc | 2 | 2 |
| acA1920-40gm | 1 | 1 |
| acA1920-40uc | 4 | 2 |
| acA1920-40ucMED | 4 | 2 |
| acA1920-40um | 4 | 1 |
| acA1920-40umMED | 4 | 1 |
| acA1920-48gc | 32 | 2 |
| acA1920-48gm | 32 | 1 |
| acA1920-50gc | 2 | 2 |
| acA1920-50gm | 1 | 1 |
| acA1920-150uc | 32 | 2 |
| acA1920-150um | 32 | 1 |
| acA1920-155uc | 4 | 2 |
| acA1920-155ucMED | 4 | 2 |
| acA1920-155um | 4 | 1 |
| acA1920-155umMED | 4 | 1 |
| acA2000-50gc | 2 | 2 |
| acA2000-50gm | 1 | 1 |
| acA2000-165uc | 8 | 2 |
| acA2000-165um | 8 | 1 |
| acA2040-25gc | 2 | 2 |
| acA2040-25gm | 1 | 1 |
| acA2040-25gmNIR | 1 | 1 |
| acA2040-35gc | 2 | 2 |
| acA2040-35gm | 1 | 1 |
| acA2040-55uc | 4 | 2 |
| acA2040-55um | 4 | 1 |
| acA2040-90uc | 8 | 2 |
| acA2040-90um | 8 | 1 |
| acA2040-90umNIR | 8 | 1 |
| acA2040-120uc | 4 | 2 |
| acA2040-120um | 4 | 1 |
| acA2440-20gc | 2 | 2 |
| acA2440-20gm | 1 | 1 |
| acA2440-35uc | 4 | 2 |
| acA2440-35ucMED | 4 | 2 |
| acA2440-35um | 4 | 1 |
| acA2440-35umMED | 4 | 1 |
| acA2440-75uc | 4 | 2 |
| acA2440-75ucMED | 4 | 2 |
| acA2440-75um | 4 | 1 |
| acA2440-75umMED | 4 | 1 |
| acA2500-14gc | 64 | 64 |
| acA2500-14gm | 64 | 64 |
| acA2500-14uc | 64a | 64a |
| acA2500-14um | 64a | 64a |
| acA2500-20gc | 32 | 2 |
| acA2500-20gcMED | 32 | 2 |
| acA2500-20gm | 32 | 1 |
| acA2500-20gmMED | 32 | 1 |
| acA2500-60uc | 32 | 1 |
| acA2500-60um | 32 | 1 |
| acA3088-16gc | 376 | 320 |
| acA3088-16gm | 376 | 320 |
| acA3088-57uc | 376 | 320 |
| acA3088-57ucMED | 376 | 320 |
| acA3088-57um | 376 | 320 |
| acA3088-57umMED | 376 | 320 |
| acA3800-10gc | 64 | 64 |
| acA3800-10gm | 64 | 64 |
| acA3800-14uc | 64 | 64 |
| acA3800-14um | 64a | 64a |
| acA4024-8gc | 8 | 6 |
| acA4024-8gm | 8 | 5 |
| acA4024-29uc | 8 | 6 |
| acA4024-29um | 8 | 5 |
| acA4096-11gc | 16 | 2 |
| acA4096-11gm | 16 | 1 |
| acA4096-30uc | 4 | 2 |
| acA4096-30ucMED | 4 | 2 |
| acA4096-30um | 4 | 1 |
| acA4096-30umMED | 4 | 1 |
| acA4096-40uc | 4 | 2 |
| acA4096-40ucMED | 4 | 2 |
| acA4096-40um | 4 | 1 |
| acA4096-40umMED | 4 | 1 |
| acA4112-8gc | 16 | 2 |
| acA4112-8gm | 16 | 1 |
| acA4112-20uc | 4 | 2 |
| acA4112-20ucMED | 4 | 2 |
| acA4112-20um | 4 | 1 |
| acA4112-20umMED | 4 | 1 |
| acA4112-30uc | 4 | 2 |
| acA4112-30ucMED | 4 | 2 |
| acA4112-30um | 4 | 1 |
| acA4112-30umMED | 4 | 1 |
| acA5472-5gc | 8 | 6 |
| acA5472-5gm | 8 | 5 |
| acA5472-17uc | 8 | 6 |
| acA5472-17ucMED | 8 | 6 |
| acA5472-17um | 8 | 5 |
| acA5472-17umMED | 8 | 5 |
| boA1936-400cc | 48 | 2 |
| boA1936-400cm | 48 | 2 |
| boA2448-250cc | 96 / 48b | 2 |
| boA2448-250cm | 48 | 2 |
| boA2832-190cc | 96 / 48b | 2 |
| boA2832-190cm | 48 | 2 |
| boA4096-93cc | 48 | 2 |
| boA4096-93cm | 48 | 2 |
| boA4096-180cc | 96 / 48b | 2 |
| boA4096-180cm | 48 | 2 |
| boA4112-68cc | 48 | 2 |
| boA4112-68cm | 48 | 2 |
| boA4500-45cc | 48 | 2 |
| boA4500-45cm | 48 | 2 |
| boA4504-100cc | 96 / 48b | 2 |
| boA4504-100cm | 96 / 48b | 2 |
| boA5120-150cc | 256 | 4 |
| boA5120-150cm | 256 | 4 |
| boA5120-230cc | 256 | 32 |
| boA5120-230cm | 256 | 32 |
| boA5320-150cc | 96 / 48b | 2 |
| boA5320-150cm | 96 / 48b | 2 |
| boA5328-100cc | 96 / 48b | 2 |
| boA5328-100cm | 96 / 48b | 2 |
| boA6500-36cc | 48 | 2 |
| boA6500-36cm | 48 | 2 |
| boA8100-16cc | 48 | 2 |
| boA8100-16cm | 48 | 2 |
| boA9344-30cc | 256 | 4 |
| boA9344-30cm | 256 | 4 |
| boA9344-70cc | 256 | 4 |
| boA9344-70cm | 256 | 4 |
| boA13440-17cm | 96 / 48b | 2 |
| daA720-520uc | 2 | 6 |
| daA720-520um | 4 | 3 |
| daA1280-54uc | 16 | 8 |
| daA1280-54um | 16 | 8 |
| daA1440-220uc | 2 | 6 |
| daA1440-220um | 4 | 3 |
| daA1600-60uc | 16 | 8 |
| daA1600-60um | 16 | 8 |
| daA1920-15um | 16 | 8 |
| daA1920-30uc | 16 | 8 |
| daA1920-30um | 16 | 8 |
| daA1920-160uc | 2 | 6 |
| daA1920-160um | 4 | 1 |
| daA2448-70uc | 2 | 6 |
| daA2448-70um | 4 | 3 |
| daA2500-14uc | 16 | 8 |
| daA2500-14um | 16 | 8 |
| daA3840-45uc | 2 | 6 |
| daA3840-45um | 4 | 4 |
| dmA720-290gc | 4 | 2 |
| dmA720-290gm | 4 | 1 |
| dmA1440-73gc | 4 | 2 |
| dmA1440-73gm | 4 | 1 |
| dmA1920-51gc | 4 | 2 |
| dmA1920-51gm | 4 | 1 |
| dmA2048-37gc | 4 | 2 |
| dmA2048-37gm | 4 | 1 |
| dmA2448-23gc | 4 | 2 |
| dmA2448-23gm | 4 | 1 |
| dmA2840-14gc | 4 | 2 |
| dmA2840-14gm | 4 | 1 |
| dmA3536-9gc | 4 | 2 |
| dmA3536-9gm | 4 | 2 |
| dmA4096-9gc | 4 | 2 |
| dmA4096-9gm | 4 | 1 |
| puA1280-54uc | 16 | 8 |
| puA1280-54um | 16 | 8 |
| puA1600-60uc | 16 | 8 |
| puA1600-60um | 16 | 8 |
| puA1920-30uc | 4 | 4 |
| puA1920-30um | 4 | 4 |
| puA2500-14uc | 4 | 4 |
| puA2500-14um | 4 | 4 |
| r2L2048-29gc | 4 | 1 |
| r2L2048-58gm | 4 | 1 |
| r2L2048-62cc | 48 | 1 |
| r2L2048-62g5c | 4 | 1 |
| r2L2048-172cm | 48 | 1 |
| r2L2048-172g5m | 4 | 1 |
| r2L4096-14gc | 4 | 1 |
| r2L4096-29gm | 4 | 1 |
| r2L4096-42cc | 48 | 1 |
| r2L4096-42g5c | 4 | 1 |
| r2L4096-84cm | 48 | 1 |
| r2L4096-84g5m | 4 | 1 |
| r2L8192-80cc | 64 | 1 |
| r2L8192-240cm | 64 | 1 |
| r2L16384-60cc | 64 | 1 |
| r2L16384-120cm | 64 | 1 |
-
When binning is enabled, the minimum width and minimum height are reduced. Values are rounded up to the nearest integer. Example: If you have configured horizontal binning by 3, the effective minimum width is 64 / 3 = 21.333 ≈ 22.
-
10-bit pixel formats / other pixel formats
Sample Code#
ace Classic/U/L GigE Cameras#
INodeMap& nodemap = camera.GetNodeMap();
// Set the width to the maximum value
int64_t maxWidth = CIntegerParameter(nodemap, "Width").GetMax();
CIntegerParameter(nodemap, "Width").SetValue(maxWidth);
// Set the height to 500
CIntegerParameter(nodemap, "Height").SetValue(500);
// Set the offset to 0,0
CIntegerParameter(nodemap, "OffsetX").SetValue(0);
CIntegerParameter(nodemap, "OffsetY").SetValue(0);
// Set the width to the maximum value
Int64 maxWidth = camera.Parameters[PLCamera.Width].GetMaximum();
camera.Parameters[PLCamera.Width].SetValue(maxWidth);
// Set the height to 500
camera.Parameters[PLCamera.Height].SetValue(500);
// Set the offset to 0,0
camera.Parameters[PLCamera.OffsetX].SetValue(0);
camera.Parameters[PLCamera.OffsetY].SetValue(0);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
int64_t maxWidth = 0;
/* Set the width to the maximum value */
errRes = PylonDeviceGetIntegerFeatureMax(hdev, "Width", &maxWidth);
CHECK(errRes);
errRes = PylonDeviceSetIntegerFeature(hdev, "Width", maxWidth);
CHECK(errRes);
/* Set the height to 500 */
errRes = PylonDeviceSetIntegerFeature(hdev, "Height", 500);
CHECK(errRes);
/* Set the offset to 0,0 */
errRes = PylonDeviceSetIntegerFeature(hdev, "OffsetX", 0);
CHECK(errRes);
errRes = PylonDeviceSetIntegerFeature(hdev, "OffsetY", 0);
CHECK(errRes);
Other Cameras#
INodeMap& nodemap = camera.GetNodeMap();
// Set the width to the maximum value
int64_t maxWidth = CIntegerParameter(nodemap, "WidthMax").GetValue();
CIntegerParameter(nodemap, "Width").SetValue(maxWidth);
// Set the height to 500
CIntegerParameter(nodemap, "Height").SetValue(500);
// Set the offset to 0
CIntegerParameter(nodemap, "OffsetX").SetValue(0);
CIntegerParameter(nodemap, "OffsetY").SetValue(0);
// Set the width to the maximum value
Int64 maxWidth = camera.Parameters[PLCamera.WidthMax].GetValue();
camera.Parameters[PLCamera.Width].SetValue(maxWidth);
// Set the height to 500
camera.Parameters[PLCamera.Height].SetValue(500);
// Set the offset to 0
camera.Parameters[PLCamera.OffsetX].SetValue(0);
camera.Parameters[PLCamera.OffsetY].SetValue(0);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
int64_t maxWidth = 0;
/* Set the width to the maximum value */
errRes = PylonDeviceGetIntegerFeature(hdev, "WidthMax", &maxWidth);
CHECK(errRes);
errRes = PylonDeviceSetIntegerFeature(hdev, "Width", maxWidth);
CHECK(errRes);
/* Set the height to 500 */
errRes = PylonDeviceSetIntegerFeature(hdev, "Height", 500);
CHECK(errRes);
/* Set the offset to 0 */
errRes = PylonDeviceSetIntegerFeature(hdev, "OffsetX", 0);
CHECK(errRes);
errRes = PylonDeviceSetIntegerFeature(hdev, "OffsetY", 0);
CHECK(errRes);
You can also use the pylon Viewer to easily set the parameters.