Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Mini Script vTool#

The Mini Script vTool allows you to run JavaScript scripts.

Download the pylon Software Suite to use the Mini Script vTool.

Mini Script vTool

How It Works#

There are two methods for loading a script in the vTool:

  • Loading from file: Use the Filename parameter to specify the path to your script file , e.g., C:\MiniScriptScripts\IntersectionPointLines.js. Then, execute the Configure command. You can find Mini Script script files in the sample code directory of pylon Data Processing (default location: C:\Program Files\Basler\pylon\Development\Samples\pylonDataProcessing).
  • Loading via Copy and Paste: Paste your script code into the input field of the Script Code parameter. Then, execute the Configure command.

For more details on how to create scripts, refer to the Mini Script Programmer's Guide that can also be found in the sample code directory of pylon Data Processing. Configured scripts are saved in the recipe file.

Configuring the vTool#

To configure the Mini Script vTool:

Mini Script vTool Settings

  1. Select the Mini Script vTool in the Workbench.
  2. In the Features - All pane, open the vTool category.
  3. In the Script Source Selector, specify the method for loading the script:
    • If you select Filename, enter the path to your script file in the Filename parameter.
    • If you select Script Code Staged, copy the contents of your script and paste it into the Script Code Staged parameter.
  4. Click Configure.

Inputs#

Inputs are defined by the code of your script.

Outputs#

Outputs are defined by the code of your script.