Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Region Combiner vTool#

The Region Combiner vTool allows you to combine two regions using logical operations.

Download the pylon Software Suite to use the Region Combiner vTool.

Region Combiner vTool

How It Works

The vTool offers the following operations:

  • AND: Regions are combined using an AND operation, i.e., creating a union of both regions.
  • OR: Regions are combined using an OR operation, i.e., creating an intersection of both regions.
  • XOR: Regions are combined using an XOR operation, i.e., creating the symmetric difference of both regions.

Inputs#

Region1#

Accepts a region from all vTools that produce a region as an output, e.g., Thresholding vTools or Matching vTools.

  • Data type: Region

Region2#

Accepts a region from all vTools that produce a region as an output, e.g., Thresholding vTools or Matching vTools.

  • Data type: Region

Outputs#

Region#

Returns the combined region of both input regions. The output region can be used by any vTool accepting regions as input.

  • Data type: Region