Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Timer#

The Timer camera feature allows you to configure a timer output signal that goes high on specific camera events and goes low after a specific duration.

Using the Feature#

The implementation of this feature varies depending on the camera:

ace 2, boost R, dart M/R, and racer 2 Cameras#

How It Works#

Two timers are available, Timer 1 and Timer 2.

This is how a timer works:

  • A trigger source event that starts the internal timer occurs.
  • A delay begins to expire.
  • An arm delay begins to expire.
  • When the delay has expired, the timer output signal goes high and stays high for the duration that you have configured.
  • When the duration has expired, the timer output signal goes low.
  • When the arm delay has expired, the camera can receive the next trigger source event.

Timer Operation

Configuring a Timer#

To configure a timer:

  1. Set the TimerSelector parameter to the desired timer, e.g., Timer1.
  2. Set the TimerDuration parameter to the desired timer duration in microseconds.
  3. Set the TimerDelay parameter to the desired timer delay in microseconds.
  4. Set the TimerTriggerArmDelay parameter to the desired arm delay in microseconds.
  5. Set the LineSelector parameter to the output line that you want to use for the timer signal.
    If the line is a GPIO line, the line must be configured as output.
  6. If you selected Timer 1 in step 1, set the LineSource parameter to Timer1Active.
  7. If you selected Timer 2 in step 1, set the LineSource parameter to Timer2Active.

Starting a Timer#

To start a timer:

  1. Set the TimerSelector parameter to the desired timer, e.g., Timer1.
  2. Set the TimerTriggerSource parameter to the source that you want to use to start the timer, e.g., Line2.
  3. If applicable, set the TimerTriggerActivation parameter to one of the following values:
    • RisingEdge (default): The timer starts when the signal rises, i.e., when the signal status changes from low to high.
    • FallingEdge: The timer starts when the signal falls, i.e., when the signal status changes from high to low.
    • AnyEdge: The timer starts when the signal falls or rises.
    • LevelHigh: The timer starts when the signal is high. When the signal changes to low, the timer stops and must be started again.
    • LevelLow: The timer starts when the signal is low. When the signal changes to high, the timer stops and must be started again.
  4. Start the timer by sending a signal on the selected trimer trigger source.

When started, the timer's status immediately changes from TimerTriggerWait to TimerActive, regardless of the delay set. However, the timer output signal will only go high after the delay has expired.

Info

The TimerTriggerActivation parameter is only available for timer trigger sources that can be high (1) or low (0), i.e., an I/O signal or an "Active" signal like ExposureActive.

Resetting a Timer#

To reset a timer, execute the TimerReset command.

The timer's status changes from TimerActive to TimerTriggerWait.

The timer can now be restarted immediately regardless of the arm delay set.

Getting the Status of a Timer#

To get the current status of a timer, get the value of the TimerStatus parameter. This parameter is read-only.

Possible values are:

  • TimerTriggerWait: The timer is waiting to be started.
  • TimerActive: The timer has been started. A timer immediately switches to this state when the trigger source event occurs, regardless of the delay set. If an arm delay is set, the timer remains in the TimerActive state until the arm delay has expired.
  • TimerIdle: The timer is idle. A timer is in this state whenever the TimerTriggerSource parameter is set o Off, i.e., the timer can't be started.

ace Classic/U/L Cameras#

How It Works#

One timer is available, Timer 1. This is how the timer works:

  • A trigger source event (e.g., Exposure Start) that starts the internal timer occurs.
  • A delay begins to expire.
  • When the delay has expired, the timer output signal goes high and stays high for the duration that you have configured.
  • When the signal's duration has expired, the timer output signal goes low.

Timer Operation

Configuring the Timer#

  1. Set the LineSelector parameter to the output line that you want to use for the timer signal.
    If the line is a GPIO line, the line must be configured as output.
  2. Set the LineSource parameter to TimerActive.
  3. Set the TimerTriggerSource parameter to one of the available trigger source events:

    • ExposureStart: The timer starts when the exposure starts.
    • FlashWindowStart: The timer starts when the flash window opens.
  4. Set the TimerDuration parameter to the desired timer duration in microseconds.

  5. Set the TimerDelay parameter to the desired timer delay in microseconds.

Info

On some camera models, you may have to increase the maximum timer duration and timer delay values.

Increasing the Maximum Timer Duration and Delay#

On some camera models, the TimerDuration and TimerDelay parameters are limited to a default maximum value of 4 095.

To increase the maximum timer duration on these models:

  1. Divide the desired timer duration by 4 095 and round up the result to the nearest integer.
    Example: Assume you want to set a timer duration of 50 000 µs. 50000 / 4095 = 12.21 ≈ 13.
  2. Set the TimerDurationTimebaseAbs parameter to the value determined in step 1, in this case 13.
  3. Set the TimerDuration parameter to the desired timer duration, in this case 50 000.
    Internally, the camera calculates the timer duration as follows: TimerDurationRaw x TimerDurationTimebaseAbs = TimerDurationAbs.

To increase the maximum timer delay on these models:

  1. Divide the desired timer delay by 4 095 and round up the result to the nearest integer.
    Example: Assume you want to set a timer delay of 6 000 µs. 6000 / 4095 = 1.47 ≈ 2.
  2. Set the TimerDelayTimebaseAbs parameter to the value determined in step 1, in this case 2.
  3. Set the TimerDelay parameter to the desired timer delay, in this case 6 000.
    Internally, the camera calculates the timer delay as follows: TimerDelayRaw x TimerDelayTimebaseAbs = TimerDelayAbs.

Info

Depending on the TimerDurationTimebaseAbs and TimerDelayTimebaseAbs parameter values, the camera may not be able to achieve the exact timer duration and delay desired.
For example, if you set the TimerDurationTimebaseAbs parameter to 13, the camera can only achieve timer durations that are a multiple of 13. Therefore, if you set the TimerDuration parameter to 50 000 and the TimerDurationTimebaseAbs parameter to 13, the camera will automatically change the setting to the nearest possible value (e.g., 49 998, which is the nearest multiple of 13).

Additional Parameters#

  • TimerSelector: Sets which timer to configure. Because Basler ace Classic/U/L cameras support only one timer, this parameter is preset and can't be changed.

Specifics#

Show all camera models

Camera Model Default Maximum Value for Timer Duration, Delay, and Trigger Arm Delay in µs
a2A640-240gmSWIR 21 474 836.47
a2A640-240umSWIR 21 472 152.45
a2A1280-80gmSWIR 21 474 836.47
a2A1280-125umSWIR 21 472 152.45
a2A1920-51gcBAS 21 474 836.47
a2A1920-51gcIP67 21 474 836.47
a2A1920-51gcPRO 21 474 836.47
a2A1920-51gmBAS 21 474 836.47
a2A1920-51gmIP67 21 474 836.47
a2A1920-51gmPRO 21 474 836.47
a2A1920-160ucBAS 21 472 152.45
a2A1920-160ucPRO 21 472 152.45
a2A1920-160umBAS 21 472 152.45
a2A1920-160umPRO 21 472 152.45
a2A1920-165g5cBAS 21 474 836.47
a2A1920-165g5mBAS 21 474 836.47
a2A2048-35gmSWIR 21 474 836.47
a2A2048-37gcBAS 21 474 836.47
a2A2048-37gcPRO 21 474 836.47
a2A2048-37gmBAS 21 474 836.47
a2A2048-37gmPRO 21 474 836.47
a2A2048-110umSWIR 21 472 152.45
a2A2048-114g5cBAS 21 474 836.47
a2A2048-114g5mBAS 21 474 836.47
a2A2048-114ucBAS 21 472 152.45
a2A2048-114ucPRO 21 472 152.45
a2A2048-114umBAS 21 472 152.45
a2A2048-114umPRO 21 472 152.45
a2A2048-173cmSWIR 21 474 836.47
a2A2440-98g5cBAS 21 474 836.47
a2A2440-98g5mBAS 21 474 836.47
a2A2448-23gcBAS 21 474 836.47
a2A2448-23gcIP67 21 474 836.47
a2A2448-23gcPRO 21 474 836.47
a2A2448-23gmBAS 21 474 836.47
a2A2448-23gmIP67 21 474 836.47
a2A2448-23gmPRO 21 474 836.47
a2A2448-75ucBAS 21 472 152.45
a2A2448-75ucPRO 21 472 152.45
a2A2448-75umBAS 21 472 152.45
a2A2448-75umPRO 21 472 152.45
a2A2448-105g5cBAS 21 474 836.47
a2A2448-105g5mBAS 21 474 836.47
a2A2448-120cc 21 474 836.47
a2A2448-120cm 21 474 836.47
a2A2448-210cc 21 474 836.47
a2A2448-210cm 21 474 836.47
a2A2560-20gmSWIR 21 474 836.47
a2A2560-70umSWIR 21 472 152.45
a2A2560-131cmSWIR 21 474 836.47
a2A2590-22gcBAS 21 474 836.47
a2A2590-22gcPRO 21 474 836.47
a2A2590-22gmBAS 21 474 836.47
a2A2590-22gmPRO 21 474 836.47
a2A2590-60ucBAS 21 472 152.45
a2A2590-60ucPRO 21 472 152.45
a2A2590-60umBAS 21 472 152.45
a2A2590-60umPRO 21 472 152.45
a2A2600-20gcBAS 21 474 836.47
a2A2600-20gcPRO 21 474 836.47
a2A2600-20gmBAS 21 474 836.47
a2A2600-20gmPRO 21 474 836.47
a2A2600-64ucBAS 21 472 152.45
a2A2600-64ucPRO 21 472 152.45
a2A2600-64umBAS 21 472 152.45
a2A2600-64umPRO 21 472 152.45
a2A2840-14gcBAS 21 474 836.47
a2A2840-14gcIP67 21 474 836.47
a2A2840-14gcPRO 21 474 836.47
a2A2840-14gmBAS 21 474 836.47
a2A2840-14gmIP67 21 474 836.47
a2A2840-14gmPRO 21 474 836.47
a2A2840-14gmUV 21 474 836.47
a2A2840-48ucBAS 21 472 152.45
a2A2840-48ucPRO 21 472 152.45
a2A2840-48umBAS 21 472 152.45
a2A2840-48umPRO 21 472 152.45
a2A2840-48umUV 21 472 152.45
a2A2840-67g5cBAS 21 474 836.47
a2A2840-67g5mBAS 21 474 836.47
a2A2840-67g5mUV 21 474 836.47
a2A2840-86cc 21 474 836.47
a2A2840-86cm 21 474 836.47
a2A3536-9gcBAS 21 474 836.47
a2A3536-9gcPRO 21 474 836.47
a2A3536-9gmBAS 21 474 836.47
a2A3536-9gmPRO 21 474 836.47
a2A3536-31ucBAS 21 472 152.45
a2A3536-31ucPRO 21 472 152.45
a2A3536-31umBAS 21 472 152.45
a2A3536-31umPRO 21 472 152.45
a2A3536-42g5cBAS 21 474 836.47
a2A3536-42g5mBAS 21 474 836.47
a2A3840-13gcBAS 21 474 836.47
a2A3840-13gcPRO 21 474 836.47
a2A3840-13gmBAS 21 474 836.47
a2A3840-13gmPRO 21 474 836.47
a2A3840-45ucBAS 21 472 152.45
a2A3840-45ucPRO 21 472 152.45
a2A3840-45umBAS 21 472 152.45
a2A3840-45umPRO 21 472 152.45
a2A4096-9gcBAS 21 474 836.47
a2A4096-9gcIP67 21 474 836.47
a2A4096-9gcPRO 21 474 836.47
a2A4096-9gmBAS 21 474 836.47
a2A4096-9gmIP67 21 474 836.47
a2A4096-9gmPRO 21 474 836.47
a2A4096-30ucBAS 21 472 152.45
a2A4096-30ucPRO 21 472 152.45
a2A4096-30umBAS 21 472 152.45
a2A4096-30umPRO 21 472 152.45
a2A4096-44g5cBAS 21 474 836.47
a2A4096-44g5mBAS 21 474 836.47
a2A4096-67cc 21 474 836.47
a2A4096-67cm 21 474 836.47
a2A4200-12gcBAS 21 474 836.47
a2A4200-12gcPRO 21 474 836.47
a2A4200-12gmBAS 21 474 836.47
a2A4200-12gmPRO 21 474 836.47
a2A4200-40ucBAS 21 472 152.45
a2A4200-40ucPRO 21 472 152.45
a2A4200-40umBAS 21 472 152.45
a2A4200-40umPRO 21 472 152.45
a2A4504-5gcBAS 21 474 836.47
a2A4504-5gcIP67 21 474 836.47
a2A4504-5gcPRO 21 474 836.47
a2A4504-5gmBAS 21 474 836.47
a2A4504-5gmIP67 21 474 836.47
a2A4504-5gmPRO 21 474 836.47
a2A4504-18ucBAS 21 472 152.45
a2A4504-18ucPRO 21 472 152.45
a2A4504-18umBAS 21 472 152.45
a2A4504-18umPRO 21 472 152.45
a2A4504-27g5cBAS 21 474 836.47
a2A4504-27g5mBAS 21 474 836.47
a2A4504-42cc 21 474 836.47
a2A4504-42cm 21 474 836.47
a2A4508-6gcBAS 21 474 836.47
a2A4508-6gcPRO 21 474 836.47
a2A4508-6gmBAS 21 474 836.47
a2A4508-6gmPRO 21 474 836.47
a2A4508-20ucBAS 21 472 152.45
a2A4508-20ucPRO 21 472 152.45
a2A4508-20umBAS 21 472 152.45
a2A4508-20umPRO 21 472 152.45
a2A5060-4gcBAS 21 474 836.47
a2A5060-4gmBAS 21 474 836.47
a2A5060-15ucBAS 21 472 152.45
a2A5060-15umBAS 21 472 152.45
a2A5060-21g5cBAS 21 474 836.47
a2A5060-21g5mBAS 21 474 836.47
a2A5060-35cc 21 474 836.47
a2A5060-35cm 21 474 836.47
a2A5320-7gcBAS 21 474 836.47
a2A5320-7gcIP67 21 474 836.47
a2A5320-7gcPRO 21 474 836.47
a2A5320-7gmBAS 21 474 836.47
a2A5320-7gmPRO 21 474 836.47
a2A5320-7gmip67 21 474 836.47
a2A5320-23ucBAS 21 472 152.45
a2A5320-23ucPRO 21 472 152.45
a2A5320-23umBAS 21 472 152.45
a2A5320-23umPRO 21 472 152.45
a2A5320-34g5cBAS 21 474 836.47
a2A5320-34g5mBAS 21 474 836.47
a2A5320-52cc 21 474 836.47
a2A5320-52cm 21 474 836.47
a2A5328-4gcBAS 21 474 836.47
a2A5328-4gcIP67 21 474 836.47
a2A5328-4gcPRO 21 474 836.47
a2A5328-4gmBAS 21 474 836.47
a2A5328-4gmIP67 21 474 836.47
a2A5328-4gmPRO 21 474 836.47
a2A5328-15ucBAS 21 472 152.45
a2A5328-15ucPRO 21 472 152.45
a2A5328-15umBAS 21 472 152.45
a2A5328-15umPRO 21 472 152.45
a2A5328-22g5cBAS 21 474 836.47
a2A5328-22g5mBAS 21 474 836.47
a2A5328-35cc 21 474 836.47
a2A5328-35cm 21 474 836.47
acA640-121gm 16 777 215
acA640-300gc 16 777 215
acA640-300gm 16 777 215
acA640-750uc 16 777 215
acA640-750um 16 777 215
acA720-290gc 16 777 215
acA720-290gm 16 777 215
acA720-520uc 16 777 215
acA720-520um 16 777 215
acA800-200gc 16 777 215
acA800-200gm 16 777 215
acA800-510uc 16 777 215
acA800-510um 16 777 215
acA1280-60gc 4 095
acA1280-60gm 4 095
acA1300-60gc 4 095
acA1300-60gm 4 095
acA1300-60gmNIR 4 095
acA1300-75gc 16 777 215
acA1300-75gm 16 777 215
acA1300-200uc 16 777 215
acA1300-200um 16 777 215
acA1440-73gc 16 777 215
acA1440-73gm 16 777 215
acA1440-220uc 16 777 215
acA1440-220um 16 777 215
acA1600-20gc 4 095
acA1600-20uc 16 777 215
acA1600-60gc 4 095
acA1600-60gm 4 095
acA1920-25gc 4 095
acA1920-25gm 4 095
acA1920-25uc 16 777 215
acA1920-25um 16 777 215
acA1920-40gc 16 777 215
acA1920-40gm 16 777 215
acA1920-40uc 16 777 215
acA1920-40ucMED 16 777 215
acA1920-40um 16 777 215
acA1920-40umMED 16 777 215
acA1920-48gc 16 777 215
acA1920-48gm 16 777 215
acA1920-50gc 16 777 215
acA1920-50gm 16 777 215
acA1920-150uc 16 777 215
acA1920-150um 16 777 215
acA1920-155uc 16 777 215
acA1920-155ucMED 16 777 215
acA1920-155um 16 777 215
acA1920-155umMED 16 777 215
acA2000-50gc 4 095
acA2000-50gm 4 095
acA2000-165uc 16 777 215
acA2000-165um 16 777 215
acA2040-25gc 4 095
acA2040-25gm 4 095
acA2040-25gmNIR 4 095
acA2040-35gc 16 777 215
acA2040-35gm 16 777 215
acA2040-55uc 16 777 215
acA2040-55um 16 777 215
acA2040-90uc 16 777 215
acA2040-90um 16 777 215
acA2040-90umNIR 16 777 215
acA2040-120uc 16 777 215
acA2040-120um 16 777 215
acA2440-20gc 16 777 215
acA2440-20gm 16 777 215
acA2440-35uc 16 777 215
acA2440-35ucMED 16 777 215
acA2440-35um 16 777 215
acA2440-35umMED 16 777 215
acA2440-75uc 16 777 215
acA2440-75ucMED 16 777 215
acA2440-75um 16 777 215
acA2440-75umMED 16 777 215
acA2500-14gc 4 095
acA2500-14gm 4 095
acA2500-14uc 16 777 215
acA2500-14um 16 777 215
acA2500-20gc 16 777 215
acA2500-20gcMED 16 777 215
acA2500-20gm 16 777 215
acA2500-20gmMED 16 777 215
acA2500-60uc 16 777 215
acA2500-60um 16 777 215
acA3088-16gc 16 777 215
acA3088-16gm 16 777 215
acA3088-57uc 16 777 215
acA3088-57ucMED 16 777 215
acA3088-57um 16 777 215
acA3088-57umMED 16 777 215
acA3800-10gc 4 095
acA3800-10gm 4 095
acA3800-14uc 16 777 215
acA3800-14um 16 777 215
acA4024-8gc 16 777 215
acA4024-8gm 16 777 215
acA4024-29uc 16 777 215
acA4024-29um 16 777 215
acA4096-11gc 16 777 215
acA4096-11gm 16 777 215
acA4096-30uc 16 777 215
acA4096-30ucMED 16 777 215
acA4096-30um 16 777 215
acA4096-30umMED 16 777 215
acA4096-40uc 16 777 215
acA4096-40ucMED 16 777 215
acA4096-40um 16 777 215
acA4096-40umMED 16 777 215
acA4112-8gc 16 777 215
acA4112-8gm 16 777 215
acA4112-20uc 16 777 215
acA4112-20ucMED 16 777 215
acA4112-20um 16 777 215
acA4112-20umMED 16 777 215
acA4112-30uc 16 777 215
acA4112-30ucMED 16 777 215
acA4112-30um 16 777 215
acA4112-30umMED 16 777 215
acA5472-5gc 16 777 215
acA5472-5gm 16 777 215
acA5472-17uc 16 777 215
acA5472-17ucMED 16 777 215
acA5472-17um 16 777 215
acA5472-17umMED 16 777 215
boA1936-400cc 21 474 836.47
boA1936-400cm 21 474 836.47
boA2448-250cc 21 474 836.47
boA2448-250cm 21 474 836.47
boA2832-190cc 21 474 836.47
boA2832-190cm 21 474 836.47
boA4096-93cc 21 474 836.47
boA4096-93cm 21 474 836.47
boA4096-180cc 21 474 836.47
boA4096-180cm 21 474 836.47
boA4112-68cc 21 474 836.47
boA4112-68cm 21 474 836.47
boA4500-45cc 21 474 836.47
boA4500-45cm 21 474 836.47
boA4504-100cc 21 474 836.47
boA4504-100cm 21 474 836.47
boA5120-150cc Timer feature not supported
boA5120-150cm Timer feature not supported
boA5120-230cc Timer feature not supported
boA5120-230cm Timer feature not supported
boA5320-150cc 21 474 836.47
boA5320-150cm 21 474 836.47
boA5328-100cc 21 474 836.47
boA5328-100cm 21 474 836.47
boA6500-36cc 21 474 836.47
boA6500-36cm 21 474 836.47
boA8100-16cc 21 474 836.47
boA8100-16cm 21 474 836.47
boA9344-30cc Timer feature not supported
boA9344-30cm Timer feature not supported
boA9344-70cc Timer feature not supported
boA9344-70cm Timer feature not supported
boA13440-17cm 21 474 836.47
daA720-520uc 21 472 152.45
daA720-520um 21 472 152.45
daA1280-54uc Timer feature not supported
daA1280-54um Timer feature not supported
daA1440-220uc 21 472 152.45
daA1440-220um 21 472 152.45
daA1600-60uc Timer feature not supported
daA1600-60um Timer feature not supported
daA1920-15um Timer feature not supported
daA1920-30uc Timer feature not supported
daA1920-30um Timer feature not supported
daA1920-160uc 21 472 152.45
daA1920-160um 21 472 152.45
daA2448-70uc 21 472 152.45
daA2448-70um 21 472 152.45
daA2500-14uc Timer feature not supported
daA2500-14um Timer feature not supported
daA3840-45uc 21 472 152.45
daA3840-45um 21 472 152.45
dmA720-290gc 21 474 836.47
dmA720-290gm 21 474 836.47
dmA1440-73gc 21 474 836.47
dmA1440-73gm 21 474 836.47
dmA1920-51gc 21 474 836.47
dmA1920-51gm 21 474 836.47
dmA2048-37gc 21 474 836.47
dmA2048-37gm 21 474 836.47
dmA2448-23gc 21 474 836.47
dmA2448-23gm 21 474 836.47
dmA2840-14gc 21 474 836.47
dmA2840-14gm 21 474 836.47
dmA3536-9gc 21 474 836.47
dmA3536-9gm 21 474 836.47
dmA4096-9gc 21 474 836.47
dmA4096-9gm 21 474 836.47
puA1280-54uc Timer feature not supported
puA1280-54um Timer feature not supported
puA1600-60uc Timer feature not supported
puA1600-60um Timer feature not supported
puA1920-30uc Timer feature not supported
puA1920-30um Timer feature not supported
puA2500-14uc Timer feature not supported
puA2500-14um Timer feature not supported
r2L2048-29gc 21 474 836.47
r2L2048-58gm 21 474 836.47
r2L2048-62cc 21 474 836.47
r2L2048-62g5c 21 474 836.47
r2L2048-172cm 21 474 836.47
r2L2048-172g5m 21 474 836.47
r2L4096-14gc 21 474 836.47
r2L4096-29gm 21 474 836.47
r2L4096-42cc 21 474 836.47
r2L4096-42g5c 21 474 836.47
r2L4096-84cm 21 474 836.47
r2L4096-84g5m 21 474 836.47
r2L8192-80cc 21 474 836.47
r2L8192-240cm 21 474 836.47
r2L16384-60cc 21 474 836.47
r2L16384-120cm 21 474 836.47

Sample Code#

ace 2, boost R, dart M/R, and racer 2 Cameras#
// Select Timer 1
camera.TimerSelector.SetValue(TimerSelector_Timer1);
// Set the timer duration to 1000 microseconds
camera.TimerDuration.SetValue(1000.0);
// Set the timer delay to 500 microseconds
camera.TimerDelay.SetValue(500.0);
// Set the timer trigger arm delay to 5000 microseconds
camera.TimerTriggerArmDelay.SetValue(5000.0);
// Select Line 2 and configure the line as output
camera.LineSelector.SetValue(LineSelector_Line2);
camera.LineMode.SetValue(LineMode_Output);
// Specify that the timer signal is output on Line 2
camera.LineSource.SetValue(LineSource_Timer1Active);
// Specify that the timer starts whenever a rising signal is detected on Line 1
camera.TimerTriggerSource.SetValue(TimerTriggerSource_Line1);
camera.TimerTriggerActivation.SetValue(TimerTriggerActivation_RisingEdge);
// Reset the timer
camera.TimerReset.Execute();
// Get the current status of the timer
TimerStatusEnums timerStatus = camera.TimerStatus.GetValue();
INodeMap& nodemap = camera.GetNodeMap();
// Select Timer 1
CEnumParameter(nodemap, "TimerSelector").SetValue("Timer1");
// Set the timer duration to 1000 microseconds
CFloatParameter(nodemap, "TimerDuration").SetValue(1000.0);
// Set the timer delay to 500 microseconds
CFloatParameter(nodemap, "TimerDelay").SetValue(500.0);
// Set the timer trigger arm delay to 5000 microseconds
CFloatParameter(nodemap, "TimerTriggerArmDelay").SetValue(5000.0);
// Select Line 2 and configure the line as output
CEnumParameter(nodemap, "LineSelector").SetValue("Line2");
CEnumParameter(nodemap, "LineMode").SetValue("Output");
// Specify that the timer signal is output on Line 2
CEnumParameter(nodemap, "LineSource").SetValue("Timer1Active");
// Specify that the timer starts whenever a rising signal is detected on Line 1
CEnumParameter(nodemap, "TimerTriggerSource").SetValue("Line1");
CEnumParameter(nodemap, "TimerTriggerActivation").SetValue("RisingEdge");
// Reset the timer
CCommandParameter(nodemap, "TimerReset").Execute();
// Get the current status of the timer
String_t timerStatus = CEnumParameter(nodemap, "TimerStatus").GetValue();
// Select Timer 1
camera.Parameters[PLCamera.TimerSelector].SetValue(PLCamera.TimerSelector.Timer1);
// Set the timer duration to 1000 microseconds
camera.Parameters[PLCamera.TimerDuration].SetValue(1000.0);
// Set the timer delay to 500 microseconds
camera.Parameters[PLCamera.TimerDelay].SetValue(500.0);
// Set the timer trigger arm delay to 5000 microseconds
camera.Parameters[PLCamera.TimerTriggerArmDelay].SetValue(5000.0);
// Select Line 2 and configure the line as output
camera.Parameters[PLCamera.LineSelector].SetValue(PLCamera.LineSelector.Line2);
camera.Parameters[PLCamera.LineMode].SetValue(PLCamera.LineMode.Output);
// Specify that the timer signal is output on Line 2
camera.Parameters[PLCamera.LineSource].SetValue(PLCamera.LineSource.Timer1Active);
// Specify that the timer starts whenever a rising signal is detected on Line 1
camera.Parameters[PLCamera.TimerTriggerSource].SetValue(PLCamera.TimerTriggerSource.Line1);
camera.Parameters[PLCamera.TimerTriggerActivation].SetValue(PLCamera.TimerTriggerActivation.RisingEdge);
// Reset the timer
camera.Parameters[PLCamera.TimerReset].Execute();
// Get the current status of the timer
string timerStatus = camera.Parameters[PLCamera.TimerStatus].GetValue();
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
size_t len = 0;
char timerStatus_str[64] = {0};
/* Select Timer 1 */
errRes = PylonDeviceFeatureFromString(hdev, "TimerSelector", "Timer1");
CHECK(errRes);
/* Set the timer duration to 1000 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "TimerDuration", 1000.0);
CHECK(errRes);
/* Set the timer delay to 500 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "TimerDelay", 500.0);
CHECK(errRes);
/* Set the timer trigger arm delay to 5000 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "TimerTriggerArmDelay", 5000.0);
CHECK(errRes);
/* Select Line 2 and configure the line as output */
errRes = PylonDeviceFeatureFromString(hdev, "LineSelector", "Line2");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "LineMode", "Output");
CHECK(errRes);
/* Specify that the timer signal is output on Line 2 */
errRes = PylonDeviceFeatureFromString(hdev, "LineSource", "Timer1Active");
CHECK(errRes);
/* Specify that the timer starts whenever a rising signal is detected on Line 1 */
errRes = PylonDeviceFeatureFromString(hdev, "TimerTriggerSource", "Line1");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "TimerTriggerActivation", "RisingEdge");
CHECK(errRes);
/* Reset the timer */
errRes = PylonDeviceExecuteCommandFeature(hdev, "TimerReset");
CHECK(errRes);
/* Get the current status of the timer */
len = sizeof(timerStatus_str);
errRes = PylonDeviceFeatureToString(hdev, "TimerStatus", timerStatus_str, &len);
CHECK(errRes);
# Select Timer 1
camera.TimerSelector.Value = "Timer1"
# Set the timer duration to 1000 microseconds
camera.TimerDuration.Value = 1000.0
# Set the timer delay to 500 microseconds
camera.TimerDelay.Value = 500.0
# Set the timer trigger arm delay to 5000 microseconds
camera.TimerTriggerArmDelay.Value = 5000.0
# Select Line 2 and configure the line as output
camera.LineSelector.Value = "Line2"
camera.LineMode.Value = "Output"
# Specify that the timer signal is output on Line 2
camera.LineSource.Value = "Timer1Active"
# Specify that the timer starts whenever a rising signal is detected on Line 1
camera.TimerTriggerSource.Value = "Line1"
camera.TimerTriggerActivation.Value = "RisingEdge"
# Reset the timer
camera.TimerReset.Execute()
# Get the current status of the timer
timerStatus = camera.TimerStatus.Value
ace Classic/U/L GigE Cameras#
// Select Line 2 (output line)
camera.LineSelector.SetValue(LineSelector_Line2);
// Specify that the timer signal is output on Line 2
camera.LineSource.SetValue(LineSource_TimerActive);
// Specify that the timer starts when exposure starts
camera.TimerTriggerSource.SetValue(TimerTriggerSource_ExposureStart);
// Set the timer duration to 1000 microseconds
camera.TimerDurationAbs.SetValue(1000.0);
// Set the timer delay to 500 microseconds
camera.TimerDelayAbs.SetValue(500.0);
INodeMap& nodemap = camera.GetNodeMap();
// Select Line 2 (output line)
CEnumParameter(nodemap, "LineSelector").SetValue("Line2");
// Specify that the timer signal is output on Line 2
CEnumParameter(nodemap, "LineSource").SetValue("TimerActive");
// Specify that the timer starts when exposure starts
CEnumParameter(nodemap, "TimerTriggerSource").SetValue("ExposureStart");
// Set the timer duration to 1000 microseconds
CFloatParameter(nodemap, "TimerDurationAbs").SetValue(1000.0);
// Set the timer delay to 500 microseconds
CFloatParameter(nodemap, "TimerDelayAbs").SetValue(500.0);
// Select Line 2 (output line)
camera.Parameters[PLCamera.LineSelector].SetValue(PLCamera.LineSelector.Line2);
// Specify that the timer signal is output on Line 2
camera.Parameters[PLCamera.LineSource].SetValue(PLCamera.LineSource.TimerActive);
// Specify that the timer starts when exposure starts
camera.Parameters[PLCamera.TimerTriggerSource].SetValue(PLCamera.TimerTriggerSource.ExposureStart);
// Set the timer duration to 1000 microseconds
camera.Parameters[PLCamera.TimerDurationAbs].SetValue(1000.0);
// Set the timer delay to 500 microseconds
camera.Parameters[PLCamera.TimerDelayAbs].SetValue(500.0);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
/* Select Line 2 (output line) */
errRes = PylonDeviceFeatureFromString(hdev, "LineSelector", "Line2");
CHECK(errRes);
/* Specify that the timer signal is output on Line 2 */
errRes = PylonDeviceFeatureFromString(hdev, "LineSource", "TimerActive");
CHECK(errRes);
/* Specify that the timer starts when exposure starts */
errRes = PylonDeviceFeatureFromString(hdev, "TimerTriggerSource", "ExposureStart");
CHECK(errRes);
/* Set the timer duration to 1000 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "TimerDurationAbs", 1000.0);
CHECK(errRes);
/* Set the timer delay to 500 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "TimerDelayAbs", 500.0);
CHECK(errRes);
# Select Line 2 (output line)
camera.LineSelector.Value = "Line2"
# Specify that the timer signal is output on Line 2
camera.LineSource.Value = "TimerActive"
# Specify that the timer starts when exposure starts
camera.TimerTriggerSource.Value = "ExposureStart"
# Set the timer duration to 1000 microseconds
camera.TimerDurationAbs.Value = 1000.0
# Set the timer delay to 500 microseconds
camera.TimerDelayAbs.Value = 500.0
Other Cameras#
// Select Line 2 (output line)
camera.LineSelector.SetValue(LineSelector_Line2);
// Specify that the timer signal is output on Line 2
camera.LineSource.SetValue(LineSource_Timer1Active);
// Specify that the timer starts when exposure starts
camera.TimerTriggerSource.SetValue(TimerTriggerSource_ExposureStart);
// Set the timer duration to 1000 microseconds
camera.TimerDuration.SetValue(1000.0);
// Set the timer delay to 500 microseconds
camera.TimerDelay.SetValue(500.0);
INodeMap& nodemap = camera.GetNodeMap();
// Select Line 2 (output line)
CEnumParameter(nodemap, "LineSelector").SetValue("Line2");
// Specify that the timer signal is output on Line 2
CEnumParameter(nodemap, "LineSource").SetValue("Timer1Active");
// Specify that the timer starts when exposure starts
CEnumParameter(nodemap, "TimerTriggerSource").SetValue("ExposureStart");
// Set the timer duration to 1000 microseconds
CFloatParameter(nodemap, "TimerDuration").SetValue(1000.0);
// Set the timer delay to 500 microseconds
CFloatParameter(nodemap, "TimerDelay").SetValue(500.0);
// Select Line 2 (output line)
camera.Parameters[PLCamera.LineSelector].SetValue(PLCamera.LineSelector.Line2);
// Specify that the timer signal is output on Line 2
camera.Parameters[PLCamera.LineSource].SetValue(PLCamera.LineSource.Timer1Active);
// Specify that the timer starts when exposure starts
camera.Parameters[PLCamera.TimerTriggerSource].SetValue(PLCamera.TimerTriggerSource.ExposureStart);
// Set the timer duration to 1000 microseconds
camera.Parameters[PLCamera.TimerDuration].SetValue(1000.0);
// Set the timer delay to 500 microseconds
camera.Parameters[PLCamera.TimerDelay].SetValue(500.0);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
/* Select Line 2 (output line) */
errRes = PylonDeviceFeatureFromString(hdev, "LineSelector", "Line2");
CHECK(errRes);
/* Specify that the timer signal is output on Line 2 */
errRes = PylonDeviceFeatureFromString(hdev, "LineSource", "Timer1Active");
CHECK(errRes);
/* Specify that the timer starts when exposure starts */
errRes = PylonDeviceFeatureFromString(hdev, "TimerTriggerSource", "ExposureStart");
CHECK(errRes);
/* Set the timer duration to 1000 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "TimerDuration", 1000.0);
CHECK(errRes);
/* Set the timer delay to 500 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "TimerDelay", 500.0);
CHECK(errRes);
# Select Line 2 (output line)
camera.LineSelector.Value = "Line2"
# Specify that the timer signal is output on Line 2
camera.LineSource.Value = "Timer1Active"
# Specify that the timer starts when exposure starts
camera.TimerTriggerSource.Value = "ExposureStart"
# Set the timer duration to 1000 microseconds
camera.TimerDuration.Value = 1000.0
# Set the timer delay to 500 microseconds
camera.TimerDelay.Value = 500.0

You can also use the pylon Viewer to easily set the parameters.