Device Information Parameters#
This topic describes the parameters and the information each parameter provides.
Using the Feature#
Standard Device Information Parameters#
All Basler cameras mentioned in this documentation provide the following device information parameters:
Parameter Name | Access (R = read-only, RW = read / write) | Description |
---|---|---|
DeviceFirmwareVersion | R | The camera's firmware version number. |
DeviceManufacturerInfo | R | The camera's manufacturer name. Usually contains an empty string. |
DeviceModelName | R | The camera's model name, e.g., acA3800-14um. |
DeviceSerialNumber | R | The camera's serial number. |
DeviceUserID | RW | Used to assign a user-defined name to a camera. The name is displayed in the Basler pylon Viewer and the Basler pylon USB Configurator. The name is also visible in the "friendly name" field of the device information objects returned by pylon's device enumeration procedure. |
DeviceVendorName | R | The camera's vendor name, e.g., Basler. |
DeviceVersion | R | The camera's version number. |
SensorHeight | R | The actual height of the camera's sensor in pixels. |
SensorWidth | R | The actual width of the camera's sensor in pixels. |
Additional Device Information Parameters#
Depending on your camera model, the following additional device information parameters are available:
Parameter Name | Access (R = read-only, RW = read / write) | Description |
---|---|---|
DeviceFamilyName | R | The identifier of the product family of the device, e.g., "Basler ace 2" |
DeviceIndicatorMode | RW | Allows you to set the behavior of the camera's status LED. To turn the status LED on, set the parameter to Active . To turn the status LED off, set the parameter to Inactive . To turn the status LED off unless an error occurs, set the parameter to ErrorStatus . |
DeviceLinkCurrentThroughput | R | The actual bandwidth currently used for data transmission in bytes per second. |
DeviceLinkSelector | RW | Allows you to select the link for data transmission. The parameter is preset to 0. Don't change this parameter. |
DeviceLinkSpeed | R | The bandwidth negotiated on the specified link in bytes per second. |
DeviceLinkThroughputLimit | RW | Specifies the maximum available bandwidth for data transmission in bytes per second. To enable the limit, set the DeviceLinkThroughputLimitMode to On .On GigE cameras, the camera automatically adjusts the inter-packet delay to set the bandwidth to the specified limit. |
DeviceLinkThroughputLimitMode | RW / R | Allows you to limit the maximum available bandwidth for data transmission. On some cameras, this parameter is read-only. If not, set the parameter to On to enable the limit. The maximum bandwidth is limited to the DeviceLinkThroughputLimit parameter value. Note that the actual bandwidth used for data transmission may be lower than the DeviceLinkThroughputLimit parameter value. |
DeviceScanType | R | The scan type of the camera's sensor (Areascan or Linescan ) |
DeviceSFNCVersionMajor | R | The major version of the Standard Features Naming Convention (SFNC) that the camera complies with, e.g., "2" for SFNC 2.3.1. |
DeviceSFNCVersionMinor | R | The minor version of the Standard Features Naming Convention (SFNC) that the camera complies with, e.g., "3" for SFNC 2.3.1. |
DeviceSFNCVersionSubMinor | R | The subminor version of the Standard Features Naming Convention (SFNC) that the camera complies with, e.g., "1" for SFNC 2.3.1. |
HeightMax | R | The maximum allowed height of the image ROI in pixels. The value adapts to the current settings for Binning, Decimation, or Scaling (if available). |
WidthMax | R | The maximum allowed width of the image ROI in pixels. The value adapts to the current settings for Binning, Decimation, or Scaling (if available). |
Specifics#
Camera Model | Additional Device Information Parameters |
---|---|
a2A1920-51gcBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A1920-51gcPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A1920-51gmBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A1920-51gmPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A1920-160ucBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A1920-160ucPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A1920-160umBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A1920-160umPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A2590-22gcBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A2590-22gcPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A2590-22gmBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A2590-22gmPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A2590-60ucBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A2590-60ucPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A2590-60umBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A2590-60umPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A3840-13gcBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A3840-13gcPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A3840-13gmBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A3840-13gmPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A3840-45ucBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A3840-45ucPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A3840-45umBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
a2A3840-45umPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
acA640-90gc | DeviceScanType WidthMax HeightMax |
acA640-90gm | DeviceScanType WidthMax HeightMax |
acA640-90uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA640-90um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA640-120gc | DeviceScanType WidthMax HeightMax |
acA640-120gm | DeviceScanType WidthMax HeightMax |
acA640-120uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA640-120um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA640-121gm | DeviceScanType WidthMax HeightMax |
acA640-300gc | DeviceScanType WidthMax HeightMax |
acA640-300gm | DeviceScanType WidthMax HeightMax |
acA640-750uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA640-750um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA720-290gc | DeviceScanType WidthMax HeightMax |
acA720-290gm | DeviceScanType WidthMax HeightMax |
acA720-520uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA720-520um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA780-75gc | DeviceScanType WidthMax HeightMax |
acA780-75gm | DeviceScanType WidthMax HeightMax |
acA800-200gc | DeviceScanType WidthMax HeightMax |
acA800-200gm | DeviceScanType WidthMax HeightMax |
acA800-510uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA800-510um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1280-60gc | DeviceScanType WidthMax HeightMax |
acA1280-60gm | DeviceScanType WidthMax HeightMax |
acA1300-22gc | DeviceScanType WidthMax HeightMax |
acA1300-22gm | DeviceScanType WidthMax HeightMax |
acA1300-30gc | DeviceScanType WidthMax HeightMax |
acA1300-30gm | DeviceScanType WidthMax HeightMax |
acA1300-30uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1300-30um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1300-60gc | DeviceScanType WidthMax HeightMax |
acA1300-60gm | DeviceScanType WidthMax HeightMax |
acA1300-60gmNIR | DeviceScanType WidthMax HeightMax |
acA1300-75gc | DeviceScanType WidthMax HeightMax |
acA1300-75gm | DeviceScanType WidthMax HeightMax |
acA1300-200uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1300-200um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1440-73gc | DeviceScanType WidthMax HeightMax |
acA1440-73gm | DeviceScanType WidthMax HeightMax |
acA1440-220uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1440-220um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1600-20gc | DeviceScanType WidthMax HeightMax |
acA1600-20gm | DeviceScanType WidthMax HeightMax |
acA1600-20uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1600-20um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1600-60gc | DeviceScanType WidthMax HeightMax |
acA1600-60gm | DeviceScanType WidthMax HeightMax |
acA1920-25gc | DeviceScanType WidthMax HeightMax |
acA1920-25gm | DeviceScanType WidthMax HeightMax |
acA1920-25uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1920-25um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1920-40gc | DeviceScanType WidthMax HeightMax |
acA1920-40gm | DeviceScanType WidthMax HeightMax |
acA1920-40uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1920-40ucMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1920-40um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1920-40umMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1920-48gc | DeviceScanType WidthMax HeightMax |
acA1920-48gm | DeviceScanType WidthMax HeightMax |
acA1920-50gc | DeviceScanType WidthMax HeightMax |
acA1920-50gm | DeviceScanType WidthMax HeightMax |
acA1920-150uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1920-150um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1920-155uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1920-155ucMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1920-155um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA1920-155umMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2000-50gc | DeviceScanType WidthMax HeightMax |
acA2000-50gm | DeviceScanType WidthMax HeightMax |
acA2000-50gmNIR | DeviceScanType WidthMax HeightMax |
acA2000-165uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2000-165um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2000-165umNIR | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2040-25gc | DeviceScanType WidthMax HeightMax |
acA2040-25gm | DeviceScanType WidthMax HeightMax |
acA2040-25gmNIR | DeviceScanType WidthMax HeightMax |
acA2040-35gc | DeviceScanType WidthMax HeightMax |
acA2040-35gm | DeviceScanType WidthMax HeightMax |
acA2040-55uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2040-55um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2040-90uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2040-90um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2040-90umNIR | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2040-120uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2040-120um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2440-20gc | DeviceScanType WidthMax HeightMax |
acA2440-20gm | DeviceScanType WidthMax HeightMax |
acA2440-35uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2440-35ucMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2440-35um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2440-35umMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2440-75uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2440-75ucMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2440-75um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2440-75umMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2500-14gc | DeviceScanType WidthMax HeightMax |
acA2500-14gm | DeviceScanType WidthMax HeightMax |
acA2500-14uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2500-14um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2500-20gc | DeviceScanType WidthMax HeightMax |
acA2500-20gcMED | DeviceScanType WidthMax HeightMax |
acA2500-20gm | DeviceScanType WidthMax HeightMax |
acA2500-20gmMED | DeviceScanType WidthMax HeightMax |
acA2500-60uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA2500-60um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA3088-16gc | DeviceScanType WidthMax HeightMax |
acA3088-16gm | DeviceScanType WidthMax HeightMax |
acA3088-57uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA3088-57um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA3800-10gc | DeviceScanType WidthMax HeightMax |
acA3800-10gm | DeviceScanType WidthMax HeightMax |
acA3800-14uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA3800-14um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA4024-8gc | DeviceScanType WidthMax HeightMax |
acA4024-8gm | DeviceScanType WidthMax HeightMax |
acA4024-29uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA4024-29um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA4096-11gc | DeviceScanType WidthMax HeightMax |
acA4096-11gm | DeviceScanType WidthMax HeightMax |
acA4096-30uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA4096-30ucMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA4096-30um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA4096-30umMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA4096-40uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA4096-40ucMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA4096-40um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA4096-40umMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA4112-8gc | DeviceScanType WidthMax HeightMax |
acA4112-8gm | DeviceScanType WidthMax HeightMax |
acA4112-20uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA4112-20ucMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA4112-20um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA4112-20umMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA4112-30uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA4112-30ucMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA4112-30um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA4112-30umMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA4600-7gc | DeviceScanType WidthMax HeightMax |
acA4600-10uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA5472-5gc | DeviceScanType WidthMax HeightMax |
acA5472-5gm | DeviceScanType WidthMax HeightMax |
acA5472-17uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
acA5472-17um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput DeviceScanType WidthMax HeightMax |
boA4096-93cc | DeviceFamilyName DeviceIndicatorMode DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
boA4096-93cm | DeviceFamilyName DeviceIndicatorMode DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
boA4112-68cc | DeviceFamilyName DeviceIndicatorMode DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
boA4112-68cm | DeviceFamilyName DeviceIndicatorMode DeviceScanType DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor HeightMax WidthMax |
daA1280-54lc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode DeviceScanType WidthMax HeightMax |
daA1280-54lm | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode DeviceScanType WidthMax HeightMax |
daA1280-54uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode DeviceScanType WidthMax HeightMax |
daA1280-54um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode DeviceScanType WidthMax HeightMax |
daA1600-60lc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode DeviceScanType WidthMax HeightMax |
daA1600-60lm | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode DeviceScanType WidthMax HeightMax |
daA1600-60uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode DeviceScanType WidthMax HeightMax |
daA1600-60um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode DeviceScanType WidthMax HeightMax |
daA1920-15um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode DeviceScanType WidthMax HeightMax |
daA1920-30uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode DeviceScanType WidthMax HeightMax |
daA1920-30um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode DeviceScanType WidthMax HeightMax |
daA2500-14lc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode DeviceScanType WidthMax HeightMax |
daA2500-14lm | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode DeviceScanType WidthMax HeightMax |
daA2500-14uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode DeviceScanType WidthMax HeightMax |
daA2500-14um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode DeviceScanType WidthMax HeightMax |
daA2500-60mc | None |
daA2500-60mci | None |
daA4200-30mci | None |
puA1280-54uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceScanType WidthMax HeightMax |
puA1280-54um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceScanType WidthMax HeightMax |
puA1600-60uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceScanType WidthMax HeightMax |
puA1600-60um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceScanType WidthMax HeightMax |
puA1920-30uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceScanType WidthMax HeightMax |
puA1920-30um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceScanType WidthMax HeightMax |
puA2500-14uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceScanType WidthMax HeightMax |
puA2500-14um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceScanType WidthMax HeightMax |
Sample Code#
// Example: Getting some of the camera's device information parameters
// Get the camera's vendor name
String_t s = camera.DeviceVendorName.GetValue();
// Get the camera's firmware version
s = camera.DeviceFirmwareVersion.GetValue();
// Get the camera's model name
s = camera.DeviceModelName.GetValue();
// Get the width of the camera's sensor
int64_t i = camera.SensorWidth.GetValue();
INodeMap& nodemap = camera.GetNodeMap();
// Example: Getting some of the camera's device information parameters
// Get the camera's vendor name
String_t s = CStringPtr(nodemap.GetNode("DeviceVendorName"))->GetValue();
// Get the camera's firmware version
s = CStringPtr(nodemap.GetNode("DeviceFirmwareVersion"))->GetValue();
// Get the camera's model name
s = CStringPtr(nodemap.GetNode("DeviceModelName"))->GetValue();
// Get the width of the camera's sensor
int64_t i = CIntegerPtr(nodemap.GetNode("SensorWidth"))->GetValue();
INodeMap& nodemap = camera.GetNodeMap();
// Example: Getting some of the camera's device information parameters
// Get the camera's vendor name
String_t s = CStringParameter(nodemap, "DeviceVendorName").GetValue();
// Get the camera's firmware version
s = CStringParameter(nodemap, "DeviceFirmwareVersion").GetValue();
// Get the camera's model name
s = CStringParameter(nodemap, "DeviceModelName").GetValue();
// Get the width of the camera's sensor
int64_t i = CIntegerParameter(nodemap, "SensorWidth").GetValue();
// Example: Getting some of the camera's device information parameters
// Get the camera's vendor name
string s = camera.Parameters[PLCamera.DeviceVendorName].GetValue();
// Get the camera's firmware version
s = camera.Parameters[PLCamera.DeviceFirmwareVersion].GetValue();
// Get the camera's model name
s = camera.Parameters[PLCamera.DeviceModelName].GetValue();
// Get the width of the camera's sensor
Int64 i = camera.Parameters[PLCamera.SensorWidth].GetValue();
// Example: Getting some of the camera's device information parameters
// Get the camera's vendor name
string s = Pylon.DeviceFeatureToString(hdev, "DeviceVendorName");
// Get the camera's firmware version
s = Pylon.DeviceFeatureToString(hdev, "DeviceFirmwareVersion");
// Get the camera's model name
s = Pylon.DeviceFeatureToString(hdev, "DeviceModelName");
// Get the width of the camera's sensor
Int64 i = Pylon.DeviceGetIntegerFeature(hdev, "SensorWidth");
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
char* s = NULL;
size_t len = 0;
int64_t i = 0;
/* Example: Getting some of the camera's device information parameters */
/* Get the camera's vendor name */
errRes = PylonDeviceFeatureToString(hdev, "DeviceVendorName", NULL, &len);
CHECK(errRes);
s = (char*) alloca(len);
errRes = PylonDeviceFeatureToString(hdev, "DeviceVendorName", s, &len);
CHECK(errRes);
/* Get the camera's firmware version */
errRes = PylonDeviceFeatureToString(hdev, "DeviceFirmwareVersion", NULL, &len);
CHECK(errRes);
s = (char*) alloca(len);
errRes = PylonDeviceFeatureToString(hdev, "DeviceFirmwareVersion", s, &len);
CHECK(errRes);
/* Get the camera's model name */
errRes = PylonDeviceFeatureToString(hdev, "DeviceModelName", NULL, &len);
CHECK(errRes);
s = (char*) alloca(len);
errRes = PylonDeviceFeatureToString(hdev, "DeviceModelName", s, &len);
CHECK(errRes);
/* Get the width of the camera's sensor */
errRes = PylonDeviceGetIntegerFeature(hdev, "SensorWidth", &i);
CHECK(errRes);
You can also use the pylon Viewer to easily set the parameters.