Basler Vision Connector Messaging: Camera Operation#
If a requested command or argument isn't supported by the Basler Vision Connector (e.g., the command in the given action field of the command is unknown), the Basler Vision Connector replies the return code 0x03000003. See also Error message codes.
Getting List of Supported Commands#
To get the full list of commands that are currently supported by the Basler Vision Connector, the client can send the following command:
JSON Payload#
| Field | Optional | Type | Description |
|---|---|---|---|
| TransactionID | Yes | String | Transaction identification |
| Action | No | String | Method called. Fixed value: GetSupportedCommands |
Response Object#
| Field | Optional | Type | Description |
|---|---|---|---|
| TransactionID | Yes | String | Transaction identification |
| ReturnCode | No | Integer | Message code following Message Codes |
| Message | Yes | String | Response message |
| SupportedCommandList | No | Array of strings | Array of commands: the possible values for the Action field |
{
"TransactionID": "123456",
"ReturnCode": 0,
"Message": "Supported commands retrieved.",
"SupportedCommandList":
[
"EnumerateDevices",
"GetStatus",
"OpenDevice",
"CloseDevice",
"StartStreaming",
"StopStreaming",
"GetParameterNames",
"GetParameters",
"SetParameters",
"SetQuickParameters",
"SoftwareTrigger",
"GetUserSets",
"LoadUserSet",
"SaveUserSet",
"SetDefaultUserSet",
"SetDeviceConfig",
"GetDeviceConfig",
"GetSupportedCommands"
]
}