Basler Vision Connector Messaging: Retrieving Camera Parameter List#
The GetParameters command is allocated to one of the following node maps:
@CameraDevice -> CInstantCamera::GetNodeMap
@CameraInstance -> CInstantCamera::GetInstantCameraNodeMap
@DeviceTransportLayer -> CInstantCamera::GetTLNodeMap
@StreamGrabber0 -> CInstantCamera::GetStreamGrabberNodeMap
@EventGrabber -> CInstantCamera::GetEventGrabberNodeMap
If no node map is defined, the @CameraDevice default node map is used. This node map represents the camera parameters. All other commands only operate on the @CameraDevice default node map.
The syntax for using the node map is as follows:
For an explanation of node maps, see the pylon API documentation.
You can find documentation about the available node maps at:
- @CameraDevice or in your camera documentation
- @CameraInstance
- @DeviceTransportLayer
- @StreamGrabber0
- @EventGrabber
JSON Payload#
| Field | Optional | Type | Description |
|---|---|---|---|
| TransactionID | Yes | String | Transaction identification |
| Action | No | String | Method called. Fixed value: GetParameters |
| DeviceID | No | String | Device identification |
| ParameterList | No | Array of string | The list of parameters to be read |
{
"TransactionID": "2345645",
"Action": "GetParameters",
"DeviceID": "548451887",
"ParameterList": [
"Width",
"@CameraDevice/Height"
]
}
Response Object#
| Field | Optional | Type | Description |
|---|---|---|---|
| TransactionID | Yes | String | Transaction identification |
| ReturnCode | No | Integer (32-bit unsigned) | Message code following Message Codes |
| Message | Yes | String | Response message |
| ParameterList | No | Parameter Object Array | Parameter object array containing the parameter details |
Parameter Object#
| Field | Optional | Type | Description |
|---|---|---|---|
| Name | No | String | Unique parameter name |
| DisplayName | Yes | String | Display name of the parameter for the user interface |
| Type | No | String | Parameter value type. Possible values: String, Integer, Float, Enumeration, Boolean, Command |
| Value | Yes | String/ Integer (64-bit signed)/ Float/ Bool | Currently defined value. For enumerations, the type of value must be a string. This parameter object isn't available if Type is Command or Readable is False. |
| IntValue | Yes | Integer (64-bit signed) | On enumerations, it's the integer defined. |
| Readable | No | Boolean | Flag indicating whether the parameter can be read. The readable flag depends on the current camera state. |
| Writable | No | Boolean | Flag indicating whether the parameter can be written. The writable flag depends on the current camera state. |
| Minimum | Yes | Integer (64-bit signed)/ Float | Minimum allowed value for numeric type parameters |
| Maximum | Yes | Integer (64-bit signed)/ Float | Maximum allowed value for numeric type parameters |
| Increment | Yes | Integer (64-bit signed)/ Float | Allowed increment for the parameter |
| Representation | Yes | String | Information about how this parameter should be represented in a user interface. This is only available for integer and float parameters. Possible values: Linear, Logarithmic, PureNumber, Boolean, HexNumber, IPV4Address, MACAddress |
| Alias | Yes | String | Name of an alias parameter. An alias parameter represents the same functionality, but in a different form. For example, a float parameter could have an integer parameter as an alias. |
| EnumEntries | Yes | Enum Entries Array | Array containing the entries available for the parameter |
Enum Entries#
| Field | Optional | Type | Description |
|---|---|---|---|
| DisplayName | Yes | String | Display name of the enum entry for the user interface |
| Value | No | String | Parameter value that needs to be set |
| IntValue | No | Integer (64-bit signed) | Integer value of the enum entry |
| Description | Yes | String | Enum entry description |
{
"TransactionID": "2345645",
"ReturnCode": 0,
"Message": "Parameters read successfully",
"ParameterList": [
{
"Name": "@CameraDevice/Width",
"DisplayName": "Width",
"Type": "Integer",
"Value": 1024,
"Writable": true,
"Minimum": 1,
"Maximum": 4096,
"Increment": 1,
"Representation": "Linear",
"Alias": "@CameraDevice/ImageWidth"
},
{
"Name": "PixelFormat",
"DisplayName": "Pixel Format",
"Type": "Enumeration",
"Value": "Mono8",
"IntValue": 17301505,
"Writable": true,
"EnumEntries": [
{
"DisplayName": "Mono 8",
"Value": "Mono8",
"IntValue": 17301505,
"Description": "This enumeration value sets the pixel format to Mono 8."
},
{
"DisplayName": "Mono 10",
"Value": "Mono10",
"IntValue": 17825795,
"Description": "This enumeration value sets the pixel format to Mono 10."
},
{
"DisplayName": "Mono 12",
"Value": "Mono12",
"IntValue": 17825797,
"Description": "This enumeration value sets the pixel format to Mono 12."
},
{
"DisplayName": "Mono 16",
"Value": "Mono16",
"IntValue": 17825799,
"Description": "This enumeration value sets the pixel format to Mono 16."
}
]
}
]
}