Basler Vision Connector Messaging: Setting Camera Parameters#
You can define enumeration parameter types using human-readable values. For example, you can set the pixel format using the Mono 8 value instead of the enumeration integer value.
For string and integer parameters, the Basler Vision Connector expects an exact match for the set value. For float parameters, a difference of no more than 1 % is allowed due to floating-point comparison. If the provided value is outside the expected range, the setting call returns an error.
If you are using a Command parameter, no value must be used.
The list of set values is returned in the response message.
The SetParameters command is allocated to one of the following node maps:
@CameraDevice -> CInstantCamera::GetNodeMap
@CameraInstance -> CInstantCamera::GetInstantCameraNodeMap
@DeviceTransportLayer -> CInstantCamera::GetTLNodeMap
@StreamGrabber0 -> CInstantCamera::GetStreamGrabberNodeMap
@EventGrabber -> CInstantCamera::GetEventGrabberNodeMap
If no node map is defined, the @CameraDevice default node map is used. This node map represents the camera parameters. All other commands only operate on the @CameraDevice default node map.
The syntax for using the node maps is as follows:
For an explanation of node maps, see the pylon API documentation.
You can find documentation about the available node maps at:
- @CameraDevice or in your camera documentation
- @CameraInstance
- @DeviceTransportLayer
- @StreamGrabber0
- @EventGrabber
JSON Payload#
| Field | Optional | Type | Description |
|---|---|---|---|
| TransactionID | Yes | String | Transaction identification |
| Action | No | String | Method called. Fixed value: SetParameters |
| DeviceID | No | String | Device identification |
| ParameterList | No | Parameter Object Array | Object to encapsulate the parameters to be updated |
Parameter Object#
| Field | Optional | Type | Description |
|---|---|---|---|
| Name | No | String | Unique parameter name |
| Valuea | Yes: for command parameters No: for all other parameters | String/ Integer (64-bit signed)/ Float/ Bool | New value. For command parameters, the Value field must not be used. For all other parameter types the Value field must be used. |
-
On enumerations, it can be the integer value or the symbolic name. See Retrieving Parameter List for further information.
{
"TransactionID": "123567",
"Action": "SetParameters",
"DeviceID": "548451887",
"ParameterList":[
{"Name": "@CameraDevice/Width", "Value": 800},
{"Name": "Height", "Value": 600},
{"Name": "PixelFormat", "Value": "Mono8"}, //Setting using the human-readable string. This could be also the correspondent enum integer.
{"Name": "TriggerSoftware"}
]
}
Response Object#
| Field | Optional | Type | Description |
|---|---|---|---|
| TransactionID | Yes | String | Transaction identification |
| ReturnCode | No | Integer (32-bit unsigned) | Message code following Message Codes |
| Message | Yes | String | Response message |
| ParameterList | No | Parameter Object Array | Object to encapsulate the parameters to be updated |
Parameter Object#
| Field | Optional | Type | Description |
|---|---|---|---|
| Name | No | String | Unique parameter name |
| Value | No | String/ Integer (64-bit signed)/ Float/ Bool | New value |