Gamma#
Using the Feature#
How It Works#
The camera applies a gamma correction value (γ) to the brightness value of each pixel according to the following formula (red pixel value (R) of a color camera shown as an example):
The maximum pixel value (Rmax) equals, e.g., 255 for 8-bit pixel formats or 1 023 for 10-bit pixel formats.
Enabling Gamma Correction#
To enable gamma correction:
- Set the
GammaEnableparameter totrue(if available). - For best results, set the
BlackLevelparameter to 0. - Set the
Gammaparameter to the desired value. The parameter's value range is 0 to ≈4.- Gamma = 1: The overall brightness remains unchanged.
- Gamma < 1: The overall brightness increases.
- Gamma > 1: The overall brightness decreases.
In all cases, black pixels (brightness = 0) and white pixels (brightness = maximum) will not be adjusted.
Info
- If you enable gamma correction and the pixel format is set to a 12-bit pixel format, some image information will be lost. Pixel data output will still be 12-bit, but the pixel values will be interpolated during the gamma correction process.
- On boA13440-17cm cameras, gamma correction can only be enabled, if the pixel format is set to an 8-bit pixel format.
Additional Parameters#
Depending on your camera model, the following additional parameters are available:
GammaEnable: Enables or disables gamma correction.GammaSelector: Allows you to select one of the following gamma correction modes:User: The gamma correction value can be set as desired. (Default.)sRGB: The camera automatically sets a gamma correction value of approximately 0.4. This value is optimized for image display on sRGB monitors.
BslColorSpaceModeorBslColorSpace: Allows you to select one of the following gamma correction modes:RGB: No additional gamma correction value is applied.sRGB: The image brightness is optimized for display on an sRGB monitor. A gamma correction value of approximately 0.4 is applied. For more information, see the footnotes in the Specifics section.
Specifics#
| Camera Model | Additional Parameters |
|---|---|
| a2A640-240gmSWIR | None |
| a2A640-240umSWIR | None |
| a2A1280-80gmSWIR | None |
| a2A1280-125umSWIR | None |
| a2A1920-51gcBAS | BslColorSpacec |
| a2A1920-51gcIP67 | BslColorSpacec |
| a2A1920-51gcPRO | BslColorSpacec |
| a2A1920-51gmBAS | None |
| a2A1920-51gmIP67 | None |
| a2A1920-51gmPRO | None |
| a2A1920-160ucBAS | BslColorSpacec |
| a2A1920-160ucPRO | BslColorSpacec |
| a2A1920-160umBAS | None |
| a2A1920-160umPRO | None |
| a2A1920-165g5cBAS | BslColorSpacec |
| a2A1920-165g5mBAS | None |
| a2A2048-35gmSWIR | None |
| a2A2048-37gcBAS | BslColorSpacec |
| a2A2048-37gcPRO | BslColorSpacec |
| a2A2048-37gmBAS | None |
| a2A2048-37gmPRO | None |
| a2A2048-110umSWIR | None |
| a2A2048-114g5cBAS | BslColorSpacec |
| a2A2048-114g5mBAS | None |
| a2A2048-114ucBAS | BslColorSpacec |
| a2A2048-114ucPRO | BslColorSpacec |
| a2A2048-114umBAS | None |
| a2A2048-114umPRO | None |
| a2A2048-173cmSWIR | None |
| a2A2440-98g5cBAS | BslColorSpacec |
| a2A2440-98g5mBAS | None |
| a2A2448-23gcBAS | BslColorSpacec |
| a2A2448-23gcIP67 | BslColorSpacec |
| a2A2448-23gcPRO | BslColorSpacec |
| a2A2448-23gmBAS | None |
| a2A2448-23gmIP67 | None |
| a2A2448-23gmPRO | None |
| a2A2448-75ucBAS | BslColorSpacec |
| a2A2448-75ucPRO | BslColorSpacec |
| a2A2448-75umBAS | None |
| a2A2448-75umPRO | None |
| a2A2448-105g5cBAS | BslColorSpacec |
| a2A2448-105g5mBAS | None |
| a2A2448-120cc | BslColorSpacec |
| a2A2448-120cm | None |
| a2A2448-210cc | BslColorSpacec |
| a2A2448-210cm | None |
| a2A2560-20gmSWIR | None |
| a2A2560-70umSWIR | None |
| a2A2560-131cmSWIR | None |
| a2A2590-22gcBAS | BslColorSpacec |
| a2A2590-22gcPRO | BslColorSpacec |
| a2A2590-22gmBAS | None |
| a2A2590-22gmPRO | None |
| a2A2590-60ucBAS | BslColorSpacec |
| a2A2590-60ucPRO | BslColorSpacec |
| a2A2590-60umBAS | None |
| a2A2590-60umPRO | None |
| a2A2600-20gcBAS | BslColorSpacec |
| a2A2600-20gcPRO | BslColorSpacec |
| a2A2600-20gmBAS | None |
| a2A2600-20gmPRO | None |
| a2A2600-64ucBAS | BslColorSpacec |
| a2A2600-64ucPRO | BslColorSpacec |
| a2A2600-64umBAS | None |
| a2A2600-64umPRO | None |
| a2A2840-14gcBAS | BslColorSpacec |
| a2A2840-14gcIP67 | BslColorSpacec |
| a2A2840-14gcPRO | BslColorSpacec |
| a2A2840-14gmBAS | None |
| a2A2840-14gmIP67 | None |
| a2A2840-14gmPRO | None |
| a2A2840-14gmUV | None |
| a2A2840-48ucBAS | BslColorSpacec |
| a2A2840-48ucPRO | BslColorSpacec |
| a2A2840-48umBAS | None |
| a2A2840-48umPRO | None |
| a2A2840-48umUV | None |
| a2A2840-67g5cBAS | BslColorSpacec |
| a2A2840-67g5mBAS | None |
| a2A2840-67g5mUV | None |
| a2A2840-86cc | BslColorSpacec |
| a2A2840-86cm | None |
| a2A3536-9gcBAS | BslColorSpacec |
| a2A3536-9gcPRO | BslColorSpacec |
| a2A3536-9gmBAS | None |
| a2A3536-9gmPRO | None |
| a2A3536-31ucBAS | BslColorSpacec |
| a2A3536-31ucPRO | BslColorSpacec |
| a2A3536-31umBAS | None |
| a2A3536-31umPRO | None |
| a2A3536-42g5cBAS | BslColorSpacec |
| a2A3536-42g5mBAS | None |
| a2A3840-13gcBAS | BslColorSpacec |
| a2A3840-13gcPRO | BslColorSpacec |
| a2A3840-13gmBAS | None |
| a2A3840-13gmPRO | None |
| a2A3840-45ucBAS | BslColorSpacec |
| a2A3840-45ucPRO | BslColorSpacec |
| a2A3840-45umBAS | None |
| a2A3840-45umPRO | None |
| a2A4096-9gcBAS | BslColorSpacec |
| a2A4096-9gcIP67 | BslColorSpacec |
| a2A4096-9gcPRO | BslColorSpacec |
| a2A4096-9gmBAS | None |
| a2A4096-9gmIP67 | None |
| a2A4096-9gmPRO | None |
| a2A4096-30ucBAS | BslColorSpacec |
| a2A4096-30ucPRO | BslColorSpacec |
| a2A4096-30umBAS | None |
| a2A4096-30umPRO | None |
| a2A4096-44g5cBAS | BslColorSpacec |
| a2A4096-44g5mBAS | None |
| a2A4096-67cc | BslColorSpacec |
| a2A4096-67cm | None |
| a2A4200-12gcBAS | BslColorSpacec |
| a2A4200-12gcPRO | BslColorSpacec |
| a2A4200-12gmBAS | None |
| a2A4200-12gmPRO | None |
| a2A4200-40ucBAS | BslColorSpacec |
| a2A4200-40ucPRO | BslColorSpacec |
| a2A4200-40umBAS | None |
| a2A4200-40umPRO | None |
| a2A4504-5gcBAS | BslColorSpacec |
| a2A4504-5gcIP67 | BslColorSpacec |
| a2A4504-5gcPRO | BslColorSpacec |
| a2A4504-5gmBAS | None |
| a2A4504-5gmIP67 | None |
| a2A4504-5gmPRO | None |
| a2A4504-18ucBAS | BslColorSpacec |
| a2A4504-18ucPRO | BslColorSpacec |
| a2A4504-18umBAS | None |
| a2A4504-18umPRO | None |
| a2A4504-27g5cBAS | BslColorSpacec |
| a2A4504-27g5mBAS | None |
| a2A4504-42cc | BslColorSpacec |
| a2A4504-42cm | None |
| a2A4508-6gcBAS | BslColorSpacec |
| a2A4508-6gcPRO | BslColorSpacec |
| a2A4508-6gmBAS | None |
| a2A4508-6gmPRO | None |
| a2A4508-20ucBAS | BslColorSpacec |
| a2A4508-20ucPRO | BslColorSpacec |
| a2A4508-20umBAS | None |
| a2A4508-20umPRO | None |
| a2A5060-4gcBAS | BslColorSpacec |
| a2A5060-4gmBAS | None |
| a2A5060-15ucBAS | BslColorSpacec |
| a2A5060-15umBAS | None |
| a2A5060-21g5cBAS | BslColorSpacec |
| a2A5060-21g5mBAS | None |
| a2A5060-35cc | BslColorSpacec |
| a2A5060-35cm | None |
| a2A5320-7gcBAS | BslColorSpacec |
| a2A5320-7gcIP67 | BslColorSpacec |
| a2A5320-7gcPRO | BslColorSpacec |
| a2A5320-7gmBAS | None |
| a2A5320-7gmPRO | None |
| a2A5320-7gmip67 | None |
| a2A5320-23ucBAS | BslColorSpacec |
| a2A5320-23ucPRO | BslColorSpacec |
| a2A5320-23umBAS | None |
| a2A5320-23umPRO | None |
| a2A5320-34g5cBAS | BslColorSpacec |
| a2A5320-34g5mBAS | None |
| a2A5320-52cc | BslColorSpacec |
| a2A5320-52cm | None |
| a2A5328-4gcBAS | BslColorSpacec |
| a2A5328-4gcIP67 | BslColorSpacec |
| a2A5328-4gcPRO | BslColorSpacec |
| a2A5328-4gmBAS | None |
| a2A5328-4gmIP67 | None |
| a2A5328-4gmPRO | None |
| a2A5328-15ucBAS | BslColorSpacec |
| a2A5328-15ucPRO | BslColorSpacec |
| a2A5328-15umBAS | None |
| a2A5328-15umPRO | None |
| a2A5328-22g5cBAS | BslColorSpacec |
| a2A5328-22g5mBAS | None |
| a2A5328-35cc | BslColorSpacec |
| a2A5328-35cm | None |
| acA640-121gm | GammaEnable GammaSelector |
| acA640-300gc | GammaEnable GammaSelector |
| acA640-300gm | GammaEnable GammaSelector |
| acA640-750uc | Nonea |
| acA640-750um | Nonea |
| acA720-290gc | GammaEnable GammaSelector |
| acA720-290gm | GammaEnable GammaSelector |
| acA720-520uc | Nonea |
| acA720-520um | Nonea |
| acA800-200gc | GammaEnable GammaSelector |
| acA800-200gm | GammaEnable GammaSelector |
| acA800-510uc | Nonea |
| acA800-510um | Nonea |
| acA1280-60gc | GammaEnable GammaSelector |
| acA1280-60gm | GammaEnable GammaSelector |
| acA1300-60gc | GammaEnable GammaSelector |
| acA1300-60gm | GammaEnable GammaSelector |
| acA1300-60gmNIR | GammaEnable GammaSelector |
| acA1300-75gc | GammaEnable GammaSelector |
| acA1300-75gm | GammaEnable GammaSelector |
| acA1300-200uc | Nonea |
| acA1300-200um | Nonea |
| acA1440-73gc | GammaEnable GammaSelector |
| acA1440-73gm | GammaEnable GammaSelector |
| acA1440-220uc | Nonea |
| acA1440-220um | Nonea |
| acA1600-20gc | GammaEnable GammaSelector |
| acA1600-20uc | Nonea |
| acA1600-60gc | GammaEnable GammaSelector |
| acA1600-60gm | GammaEnable GammaSelector |
| acA1920-25gc | GammaEnable GammaSelector |
| acA1920-25gm | GammaEnable GammaSelector |
| acA1920-25uc | Nonea |
| acA1920-25um | Nonea |
| acA1920-40gc | GammaEnable GammaSelector |
| acA1920-40gm | GammaEnable GammaSelector |
| acA1920-40uc | Nonea |
| acA1920-40ucMED | Nonea |
| acA1920-40um | Nonea |
| acA1920-40umMED | Nonea |
| acA1920-48gc | GammaEnable GammaSelector |
| acA1920-48gm | GammaEnable GammaSelector |
| acA1920-50gc | GammaEnable GammaSelector |
| acA1920-50gm | GammaEnable GammaSelector |
| acA1920-150uc | Nonea |
| acA1920-150um | Nonea |
| acA1920-155uc | Nonea |
| acA1920-155ucMED | Nonea |
| acA1920-155um | Nonea |
| acA1920-155umMED | Nonea |
| acA2000-50gc | GammaEnable GammaSelector |
| acA2000-50gm | GammaEnable GammaSelector |
| acA2000-165uc | Nonea |
| acA2000-165um | Nonea |
| acA2040-25gc | GammaEnable GammaSelector |
| acA2040-25gm | GammaEnable GammaSelector |
| acA2040-25gmNIR | GammaEnable GammaSelector |
| acA2040-35gc | GammaEnable GammaSelector |
| acA2040-35gm | GammaEnable GammaSelector |
| acA2040-55uc | Nonea |
| acA2040-55um | Nonea |
| acA2040-90uc | Nonea |
| acA2040-90um | Nonea |
| acA2040-90umNIR | Nonea |
| acA2040-120uc | Nonea |
| acA2040-120um | Nonea |
| acA2440-20gc | GammaEnable GammaSelector |
| acA2440-20gm | GammaEnable GammaSelector |
| acA2440-35uc | Nonea |
| acA2440-35ucMED | Nonea |
| acA2440-35um | Nonea |
| acA2440-35umMED | Nonea |
| acA2440-75uc | Nonea |
| acA2440-75ucMED | Nonea |
| acA2440-75um | Nonea |
| acA2440-75umMED | Nonea |
| acA2500-14gc | GammaEnable GammaSelector |
| acA2500-14gm | GammaEnable GammaSelector |
| acA2500-14uc | Nonea |
| acA2500-14um | Nonea |
| acA2500-20gc | GammaEnable GammaSelector |
| acA2500-20gcMED | GammaEnable GammaSelector |
| acA2500-20gm | GammaEnable GammaSelector |
| acA2500-20gmMED | GammaEnable GammaSelector |
| acA2500-60uc | Nonea |
| acA2500-60um | Nonea |
| acA3088-16gc | GammaEnable GammaSelector |
| acA3088-16gm | GammaEnable GammaSelector |
| acA3088-57uc | Nonea |
| acA3088-57ucMED | Nonea |
| acA3088-57um | Nonea |
| acA3088-57umMED | Nonea |
| acA3800-10gc | GammaEnable GammaSelector |
| acA3800-10gm | GammaEnable GammaSelector |
| acA3800-14uc | Nonea |
| acA3800-14um | Nonea |
| acA4024-8gc | GammaEnable GammaSelector |
| acA4024-8gm | GammaEnable GammaSelector |
| acA4024-29uc | Nonea |
| acA4024-29um | Nonea |
| acA4096-11gc | GammaEnable GammaSelector |
| acA4096-11gm | GammaEnable GammaSelector |
| acA4096-30uc | Nonea |
| acA4096-30ucMED | Nonea |
| acA4096-30um | Nonea |
| acA4096-30umMED | Nonea |
| acA4096-40uc | Nonea |
| acA4096-40ucMED | Nonea |
| acA4096-40um | Nonea |
| acA4096-40umMED | Nonea |
| acA4112-8gc | GammaEnable GammaSelector |
| acA4112-8gm | GammaEnable GammaSelector |
| acA4112-20uc | Nonea |
| acA4112-20ucMED | Nonea |
| acA4112-20um | Nonea |
| acA4112-20umMED | Nonea |
| acA4112-30uc | Nonea |
| acA4112-30ucMED | Nonea |
| acA4112-30um | Nonea |
| acA4112-30umMED | Nonea |
| acA5472-5gc | GammaEnable GammaSelector |
| acA5472-5gm | GammaEnable GammaSelector |
| acA5472-17uc | Nonea |
| acA5472-17ucMED | Nonea |
| acA5472-17um | Nonea |
| acA5472-17umMED | Nonea |
| boA1936-400cc | BslColorSpacec |
| boA1936-400cm | None |
| boA2448-250cc | BslColorSpacec |
| boA2448-250cm | None |
| boA2832-190cc | BslColorSpacec |
| boA2832-190cm | None |
| boA4096-93cc | BslColorSpacec |
| boA4096-93cm | None |
| boA4096-180cc | BslColorSpacec |
| boA4096-180cm | None |
| boA4112-68cc | BslColorSpacec |
| boA4112-68cm | None |
| boA4500-45cc | BslColorSpacec |
| boA4500-45cm | None |
| boA4504-100cc | BslColorSpacec |
| boA4504-100cm | None |
| boA5120-150cc | Gamma feature not supported |
| boA5120-150cm | Gamma feature not supported |
| boA5120-230cc | Gamma feature not supported |
| boA5120-230cm | Gamma feature not supported |
| boA5320-150cc | BslColorSpacec |
| boA5320-150cm | None |
| boA5328-100cc | BslColorSpacec |
| boA5328-100cm | None |
| boA6500-36cc | BslColorSpacec |
| boA6500-36cm | None |
| boA8100-16cc | BslColorSpacec |
| boA8100-16cm | None |
| boA9344-30cc | Gamma feature not supported |
| boA9344-30cm | Gamma feature not supported |
| boA9344-70cc | Gamma feature not supported |
| boA9344-70cm | Gamma feature not supported |
| boA13440-17cm | None |
| daA720-520uc | BslColorSpacea |
| daA720-520um | None |
| daA1280-54uc | BslColorSpaceModeb |
| daA1280-54um | None |
| daA1440-220uc | BslColorSpacea |
| daA1440-220um | None |
| daA1600-60uc | BslColorSpaceModeb |
| daA1600-60um | None |
| daA1920-15um | None |
| daA1920-30uc | BslColorSpaceModeb |
| daA1920-30um | None |
| daA1920-160uc | BslColorSpacea |
| daA1920-160um | None |
| daA2448-70uc | BslColorSpacea |
| daA2448-70um | None |
| daA2500-14uc | BslColorSpaceModeb |
| daA2500-14um | None |
| daA3840-45uc | BslColorSpacea |
| daA3840-45um | None |
| dmA720-290gc | BslColorSpacec |
| dmA720-290gm | None |
| dmA1440-73gc | BslColorSpacec |
| dmA1440-73gm | None |
| dmA1920-51gc | BslColorSpacec |
| dmA1920-51gm | None |
| dmA2048-37gc | BslColorSpacec |
| dmA2048-37gm | None |
| dmA2448-23gc | BslColorSpacec |
| dmA2448-23gm | None |
| dmA2840-14gc | BslColorSpacec |
| dmA2840-14gm | None |
| dmA3536-9gc | BslColorSpacec |
| dmA3536-9gm | None |
| dmA4096-9gc | BslColorSpacec |
| dmA4096-9gm | None |
| puA1280-54uc | BslColorSpaceModeb |
| puA1280-54um | None |
| puA1600-60uc | BslColorSpaceModeb |
| puA1600-60um | None |
| puA1920-30uc | BslColorSpaceModeb |
| puA1920-30um | None |
| puA2500-14uc | BslColorSpaceModeb |
| puA2500-14um | None |
| r2L2048-29gc | BslColorSpacec |
| r2L2048-58gm | None |
| r2L2048-62cc | BslColorSpacec |
| r2L2048-62g5c | BslColorSpacec |
| r2L2048-172cm | None |
| r2L2048-172g5m | None |
| r2L4096-14gc | BslColorSpacec |
| r2L4096-29gm | None |
| r2L4096-42cc | BslColorSpacec |
| r2L4096-42g5c | BslColorSpacec |
| r2L4096-84cm | None |
| r2L4096-84g5m | None |
| r2L8192-80cc | BslColorSpacec |
| r2L8192-240cm | None |
| r2L16384-60cc | BslColorSpacec |
| r2L16384-120cm | None |
-
If you select a light source preset, an additional gamma correction value of approximately 0.4 is applied (sRGB gamma correction). This value is applied separately and not included in the
Gammaparameter value. Example: You have set the light source preset to Tungsten and theGammaparameter value to 1.2. First, an automatic correction value of approximately 0.4 is applied to the pixel values. After that, a gamma correction value of 1.2 is applied to the resulting pixel values. -
Only available if the pixel format is set to YCbCr422 or RGB8.
-
If the color space is set to
sRGB, a gamma correction value of approximately 0.4 is applied. This value is applied separately and not included in theGammaparameter value. Example: You set the color space to sRGB and theGammaparameter to 1.2. First, an automatic correction value of approximately 0.4 is applied to the pixel values. After that, a gamma correction value of 1.2 is applied to the resulting pixel values.
If you have selected a Light Source Preset, setting the color space tosRGBwill also affect the Balance White, Color Adjustment, and Color Transformation features. -
If the color space is set to
sRGB, a gamma correction value of approximately 0.4 is applied, theGammaparameter becomes read-only, and theGammaparameter value is ignored.
Sample Code#
ace 2, boost, and dart R Cameras#
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Set the Gamma value to 1.2 */
errRes = PylonDeviceSetFloatFeature(hdev, "Gamma", 1.2);
CHECK(errRes);
/* Set the color space to sRGB */
errRes = PylonDeviceFeatureFromString(hdev, "BslColorSpace", "sRGB");
CHECK(errRes);
ace Classic/U/L GigE Cameras#
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Enable the Gamma feature */
errRes = PylonDeviceSetBooleanFeature(hdev, "GammaEnable", 1);
CHECK(errRes);
/* Set the gamma type to User */
errRes = PylonDeviceFeatureFromString(hdev, "GammaSelector", "User");
CHECK(errRes);
/* Set the Gamma value to 1.2 */
errRes = PylonDeviceSetFloatFeature(hdev, "Gamma", 1.2);
CHECK(errRes);
Other Cameras#
You can also use the pylon Viewer to easily set the parameters.