Network-Related Parameters#
Using the Feature#
Available Parameters#
Depending on your camera model, the following network-related parameters are available:
| Parameter Name | Display Name | Description |
|---|---|---|
| BandwidthReserveMode | Bandwidth Reserve Mode | Allows you to configure the bandwidth reserve and bandwidth reserve accumulation (see below) in a single step. You can set the parameter to the following values:
|
| BslDeviceLinkCurrentThroughput | Device Link Current Throughput | Indicates the actual bandwidth (in bytes per second) that the camera uses to transmit image data and chunk data given the current camera settings. If you are using the Acquisition Frame Rate parameter to control the camera's frame rate, the camera uses that parameter value to calculate the throughput. If you are using software triggering or hardware triggering to control the camera's frame rate, the camera uses the maximum possible frame rate with the current camera settings to calculate the throughput. This parameter is read-only. |
| DeviceLinkThroughputLimit | Device Link Throughput Limit | Allows you to limit the maximum available bandwidth for data transmission. For more information, see Device Information Parameters. |
| GevHeartbeatTimeout | Heartbeat Timeout | Sets the heartbeat timeout (in milliseconds). If a timeout occurs, the camera releases the network connection and enters a state that allows reconnection. By default, the heartbeat timeout is set to 3000 ms. Changing the value is not required for normal camera operation. However, if you are debugging an application and stop at a break point, a heartbeat timeout may occur and the connection to the camera may be lost. Therefore, you should increase the GevHeartbeatTimeout parameter value while debugging. When debugging is complete, you should return the timeout to its normal setting.For more information, see the Debugging pylon Applications Using GigE Cameras section in the pylon API Documentation.a |
| GevSCBWA | Bandwidth Assigned | Indicates the bandwidth in bytes per second that can be used by the camera to transmit image and chunk data, to handle packet resends, and to control data transmission. The assigned bandwidth can be adjusted by changing the inter-packet delay and the frame transmission delay settings. This parameter is read-only. |
| GevSCBWR | Bandwidth Reserve | Specifies which portion of the assigned bandwidth is reserved to handle packet resends and to control data transmission. The setting is expressed as a percentage of the assigned bandwidth. Example: If a bandwidth of 30 MByte/s is assigned to the camera and the GevSCBWR parameter is set to 5 %, the bandwidth reserve will be 1.5 MByte/s. |
| GevSCBWRA | Bandwidth Reserve Accumulation | Multiplier used to set the maximum number of resends that can be held in the "accumulator pool". You can use the GevSCBWRA parameter to handle situations when the network connection becomes unstable, e.g., because of a sudden EMI burst. In these situations, a larger number of packet resends may be needed to transmit an image. The bandwidth reserve accumulation is basically an extra pool of resends that the camera can use in unusual situations.Example: Assume that the current bandwidth reserve setting is large enough to allow up to 5 packet resends during a frame period. Also assume that the bandwidth reserve accumulation ( GevSCBWRA parameter) is set to 3. With these settings, the accumulator pool can hold a maximum of 5 x 3 = 15 resends. |
| GevSCDCT | Device Current Throughput | See Device Link Current Throughput. |
| GevSCDMT | Device Max Throughput | Indicates the maximum amount of data (in bytes per second) that the camera is theoretically able to generate given its current settings and under ideal conditions without network restrictions. This parameter doesn't take into account whether the GigE network has the capacity to carry all of the data and does not consider any bandwidth required for resends. If you are using the Acquisition Frame Rate parameter to control the camera's frame rate, the camera uses that parameter value to calculate the GevSCDMT parameter value. If you are using software triggering or hardware triggering to control the camera's frame rate, the camera uses the maximum frame rate allowed with the current camera settings to calculate the GevSCDMT parameter value.This parameter is read-only. |
| GevSCFJM | Frame Jitter Max | Indicates the maximum time in ticksb that the next frame transmission could be delayed due to a burst of resends. If the bandwidth reserve accumulation is set to a high value, the camera can experience a large burst of data resends during the transmission of a frame. This burst of resends will delay the start of the transmission of the next acquired frame. This parameter is read-only. |
| GevSCFTD | Frame Transmission Delay | Sets a delay in ticksb between when a camera would normally begin transmitting an acquired frame and when it actually begins transmission. In most cases, this parameter should be set to zero. However, if your network hardware can't handle spikes in network traffic (e.g., if you are triggering multiple cameras simultaneously), you can use the frame transmission delay parameter to stagger the start of image data transmissions from each camera. |
| GevSCPD | Inter-Packet Delay | Sets the inter-packet delay in ticksb. If your network hardware can't handle the incoming packet rate, it is useful to increase the delay between packet transmissions. This may reduce the amount of dropped packets. Note that this also slows the data transmission. As a result, the camera's frame rate may decrease. |
| GevSCPSPacketSize | Packet Size | Specifies the maximum size of a data packet transmitted via Ethernet. The value is in bytes. The parameter should always be set to the maximum size that your network hardware can handle. By default, the packet size is set to 1 500 bytes. This will be sufficient for most configurations.c If required, you can increase the packet size to reduce Ethernet overhead load and improve network efficiency. The size of the leader and the trailer always remains the same, regardless of the packet size. You should bear in mind that the last data packet is, in most cases, smaller than the others. |
| GevStreamChannelSelector | Stream Channel Selector | Specifies the stream channel that will be affected when other network related parameters are changed. The GigE Vision standard specifies a mechanism for establishing several separate stream channels between the camera and the computer. Currently, the cameras support only one stream channel, i.e., stream channel 0. Therefore, the GevStreamChannelSelector parameter is preset to StreamChannel0 and can't be changed. |
| PayloadSize | Payload Size | Indicates the total size in bytes of the image data plus any chunk data transmitted. Packet headers are not included. This parameter is read-only. |
-
The pylon API also provides a
HeartbeatTimeoutparameter that sets the heartbeat timeout on transport layer side. TheHeartbeatTimeoutandGevHeartbeatTimeoutparameters are automatically synchronized. When you change one parameter, the other one adapts, and vice versa. -
On ace Classic/U/L cameras, one tick equals 8 ns (PTP disabled) or 1 ns (PTP enabled). On other cameras, one tick always equals 1 ns. You can determine the tick frequency by reading the
GevTimestampTickFrequencyparameter value. This value indicates the number of clock ticks per second. -
If you increase the packet size above 1 500 bytes, you must enable the so-called Jumbo Frames support on all network devices involved including any switches. Whenever you increase the packet size on the camera side, you must also adjust the packet size of your network controller card. Otherwise, streaming may fail due to blocked packets.
Specifics#
| Camera Model | Available Parameters |
|---|---|
| a2A640-240gmSWIR | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A640-240umSWIR | Feature not supported |
| a2A1280-80gmSWIR | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A1280-125umSWIR | Feature not supported |
| a2A1920-51gcBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A1920-51gcIP67 | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A1920-51gcPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A1920-51gmBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A1920-51gmIP67 | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A1920-51gmPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A1920-160ucBAS | Feature not supported |
| a2A1920-160ucPRO | Feature not supported |
| a2A1920-160umBAS | Feature not supported |
| a2A1920-160umPRO | Feature not supported |
| a2A1920-165g5cBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A1920-165g5mBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2048-35gmSWIR | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2048-37gcBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2048-37gcPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2048-37gmBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2048-37gmPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2048-110umSWIR | Feature not supported |
| a2A2048-114g5cBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2048-114g5mBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2048-114ucBAS | Feature not supported |
| a2A2048-114ucPRO | Feature not supported |
| a2A2048-114umBAS | Feature not supported |
| a2A2048-114umPRO | Feature not supported |
| a2A2048-173cmSWIR | Feature not supported |
| a2A2440-98g5cBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2440-98g5mBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2448-23gcBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2448-23gcIP67 | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2448-23gcPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2448-23gmBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2448-23gmIP67 | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2448-23gmPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2448-75ucBAS | Feature not supported |
| a2A2448-75ucPRO | Feature not supported |
| a2A2448-75umBAS | Feature not supported |
| a2A2448-75umPRO | Feature not supported |
| a2A2448-105g5cBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2448-105g5mBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2448-120cc | Feature not supported |
| a2A2448-120cm | Feature not supported |
| a2A2448-210cc | Feature not supported |
| a2A2448-210cm | Feature not supported |
| a2A2560-20gmSWIR | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2560-70umSWIR | Feature not supported |
| a2A2560-131cmSWIR | Feature not supported |
| a2A2590-22gcBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2590-22gcPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2590-22gmBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2590-22gmPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2590-60ucBAS | Feature not supported |
| a2A2590-60ucPRO | Feature not supported |
| a2A2590-60umBAS | Feature not supported |
| a2A2590-60umPRO | Feature not supported |
| a2A2600-20gcBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2600-20gcPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2600-20gmBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2600-20gmPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2600-64ucBAS | Feature not supported |
| a2A2600-64ucPRO | Feature not supported |
| a2A2600-64umBAS | Feature not supported |
| a2A2600-64umPRO | Feature not supported |
| a2A2840-14gcBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2840-14gcIP67 | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2840-14gcPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2840-14gmBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2840-14gmIP67 | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2840-14gmPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2840-14gmUV | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2840-48ucBAS | Feature not supported |
| a2A2840-48ucPRO | Feature not supported |
| a2A2840-48umBAS | Feature not supported |
| a2A2840-48umPRO | Feature not supported |
| a2A2840-48umUV | Feature not supported |
| a2A2840-67g5cBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2840-67g5mBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2840-67g5mUV | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A2840-86cc | Feature not supported |
| a2A2840-86cm | Feature not supported |
| a2A3536-9gcBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A3536-9gcPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A3536-9gmBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A3536-9gmPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A3536-31ucBAS | Feature not supported |
| a2A3536-31ucPRO | Feature not supported |
| a2A3536-31umBAS | Feature not supported |
| a2A3536-31umPRO | Feature not supported |
| a2A3536-42g5cBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A3536-42g5mBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A3840-13gcBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A3840-13gcPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A3840-13gmBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A3840-13gmPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A3840-45ucBAS | Feature not supported |
| a2A3840-45ucPRO | Feature not supported |
| a2A3840-45umBAS | Feature not supported |
| a2A3840-45umPRO | Feature not supported |
| a2A4096-9gcBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4096-9gcIP67 | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4096-9gcPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4096-9gmBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4096-9gmIP67 | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4096-9gmPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4096-30ucBAS | Feature not supported |
| a2A4096-30ucPRO | Feature not supported |
| a2A4096-30umBAS | Feature not supported |
| a2A4096-30umPRO | Feature not supported |
| a2A4096-44g5cBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4096-44g5mBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4096-67cc | Feature not supported |
| a2A4096-67cm | Feature not supported |
| a2A4200-12gcBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4200-12gcPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4200-12gmBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4200-12gmPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize GevtreamChannelSelector PayloadSize |
| a2A4200-40ucBAS | Feature not supported |
| a2A4200-40ucPRO | Feature not supported |
| a2A4200-40umBAS | Feature not supported |
| a2A4200-40umPRO | Feature not supported |
| a2A4504-5gcBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4504-5gcIP67 | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4504-5gcPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4504-5gmBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4504-5gmIP67 | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4504-5gmPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4504-18ucBAS | Feature not supported |
| a2A4504-18ucPRO | Feature not supported |
| a2A4504-18umBAS | Feature not supported |
| a2A4504-18umPRO | Feature not supported |
| a2A4504-27g5cBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4504-27g5mBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4504-42cc | Feature not supported |
| a2A4504-42cm | Feature not supported |
| a2A4508-6gcBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4508-6gcPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4508-6gmBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4508-6gmPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A4508-20ucBAS | Feature not supported |
| a2A4508-20ucPRO | Feature not supported |
| a2A4508-20umBAS | Feature not supported |
| a2A4508-20umPRO | Feature not supported |
| a2A5060-4gcBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5060-4gmBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5060-15ucBAS | Feature not supported |
| a2A5060-15umBAS | Feature not supported |
| a2A5060-21g5cBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5060-21g5mBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5060-35cc | Feature not supported |
| a2A5060-35cm | Feature not supported |
| a2A5320-7gcBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5320-7gcIP67 | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5320-7gcPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5320-7gmBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5320-7gmPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5320-7gmip67 | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5320-23ucBAS | Feature not supported |
| a2A5320-23ucPRO | Feature not supported |
| a2A5320-23umBAS | Feature not supported |
| a2A5320-23umPRO | Feature not supported |
| a2A5320-34g5cBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5320-34g5mBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5320-52cc | Feature not supported |
| a2A5320-52cm | Feature not supported |
| a2A5328-4gcBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5328-4gcIP67 | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5328-4gcPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5328-4gmBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5328-4gmIP67 | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5328-4gmPRO | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5328-15ucBAS | Feature not supported |
| a2A5328-15ucPRO | Feature not supported |
| a2A5328-15umBAS | Feature not supported |
| a2A5328-15umPRO | Feature not supported |
| a2A5328-22g5cBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5328-22g5mBAS | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| a2A5328-35cc | Feature not supported |
| a2A5328-35cm | Feature not supported |
| acA640-121gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA640-300gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA640-300gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA640-750uc | Feature not supported |
| acA640-750um | Feature not supported |
| acA720-290gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA720-290gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA720-520uc | Feature not supported |
| acA720-520um | Feature not supported |
| acA800-200gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA800-200gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA800-510uc | Feature not supported |
| acA800-510um | Feature not supported |
| acA1280-60gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1280-60gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1300-60gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1300-60gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1300-60gmNIR | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1300-75gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1300-75gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1300-200uc | Feature not supported |
| acA1300-200um | Feature not supported |
| acA1440-73gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1440-73gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1440-220uc | Feature not supported |
| acA1440-220um | Feature not supported |
| acA1600-20gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1600-20uc | Feature not supported |
| acA1600-60gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1600-60gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1920-25gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1920-25gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1920-25uc | Feature not supported |
| acA1920-25um | Feature not supported |
| acA1920-40gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1920-40gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1920-40uc | Feature not supported |
| acA1920-40ucMED | Feature not supported |
| acA1920-40um | Feature not supported |
| acA1920-40umMED | Feature not supported |
| acA1920-48gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1920-48gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1920-50gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1920-50gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA1920-150uc | Feature not supported |
| acA1920-150um | Feature not supported |
| acA1920-155uc | Feature not supported |
| acA1920-155ucMED | Feature not supported |
| acA1920-155um | Feature not supported |
| acA1920-155umMED | Feature not supported |
| acA2000-50gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA2000-50gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA2000-165uc | Feature not supported |
| acA2000-165um | Feature not supported |
| acA2040-25gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA2040-25gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA2040-25gmNIR | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA2040-35gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA2040-35gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA2040-55uc | Feature not supported |
| acA2040-55um | Feature not supported |
| acA2040-90uc | Feature not supported |
| acA2040-90um | Feature not supported |
| acA2040-90umNIR | Feature not supported |
| acA2040-120uc | Feature not supported |
| acA2040-120um | Feature not supported |
| acA2440-20gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA2440-20gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA2440-35uc | Feature not supported |
| acA2440-35ucMED | Feature not supported |
| acA2440-35um | Feature not supported |
| acA2440-35umMED | Feature not supported |
| acA2440-75uc | Feature not supported |
| acA2440-75ucMED | Feature not supported |
| acA2440-75um | Feature not supported |
| acA2440-75umMED | Feature not supported |
| acA2500-14gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA2500-14gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA2500-14uc | Feature not supported |
| acA2500-14um | Feature not supported |
| acA2500-20gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA2500-20gcMED | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA2500-20gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA2500-20gmMED | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA2500-60uc | Feature not supported |
| acA2500-60um | Feature not supported |
| acA3088-16gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA3088-16gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA3088-57uc | Feature not supported |
| acA3088-57ucMED | Feature not supported |
| acA3088-57um | Feature not supported |
| acA3088-57umMED | Feature not supported |
| acA3800-10gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA3800-10gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA3800-14uc | Feature not supported |
| acA3800-14um | Feature not supported |
| acA4024-8gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA4024-8gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA4024-29uc | Feature not supported |
| acA4024-29um | Feature not supported |
| acA4096-11gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA4096-11gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA4096-30uc | Feature not supported |
| acA4096-30ucMED | Feature not supported |
| acA4096-30um | Feature not supported |
| acA4096-30umMED | Feature not supported |
| acA4096-40uc | Feature not supported |
| acA4096-40ucMED | Feature not supported |
| acA4096-40um | Feature not supported |
| acA4096-40umMED | Feature not supported |
| acA4112-8gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA4112-8gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA4112-20uc | Feature not supported |
| acA4112-20ucMED | Feature not supported |
| acA4112-20um | Feature not supported |
| acA4112-20umMED | Feature not supported |
| acA4112-30uc | Feature not supported |
| acA4112-30ucMED | Feature not supported |
| acA4112-30um | Feature not supported |
| acA4112-30umMED | Feature not supported |
| acA5472-5gc | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA5472-5gm | GevHeartbeatTimeout GevSCBWA GevSCBWR GevSCBWRA GevSCDCT GevSCDMT GevSCFJM GevSCFTD GevSCPD GevSCPSPacketSize GevStreamChannelSelector PayloadSize |
| acA5472-17uc | Feature not supported |
| acA5472-17ucMED | Feature not supported |
| acA5472-17um | Feature not supported |
| acA5472-17umMED | Feature not supported |
| boA1936-400cc | Feature not supported |
| boA1936-400cm | Feature not supported |
| boA2448-250cc | Feature not supported |
| boA2448-250cm | Feature not supported |
| boA2832-190cc | Feature not supported |
| boA2832-190cm | Feature not supported |
| boA4096-93cc | Feature not supported |
| boA4096-93cm | Feature not supported |
| boA4096-180cc | Feature not supported |
| boA4096-180cm | Feature not supported |
| boA4112-68cc | Feature not supported |
| boA4112-68cm | Feature not supported |
| boA4500-45cc | Feature not supported |
| boA4500-45cm | Feature not supported |
| boA4504-100cc | Feature not supported |
| boA4504-100cm | Feature not supported |
| boA5120-150cc | Feature not supported |
| boA5120-150cm | Feature not supported |
| boA5120-230cc | Feature not supported |
| boA5120-230cm | Feature not supported |
| boA5320-150cc | Feature not supported |
| boA5320-150cm | Feature not supported |
| boA5328-100cc | Feature not supported |
| boA5328-100cm | Feature not supported |
| boA6500-36cc | Feature not supported |
| boA6500-36cm | Feature not supported |
| boA8100-16cc | Feature not supported |
| boA8100-16cm | Feature not supported |
| boA9344-30cc | Feature not supported |
| boA9344-30cm | Feature not supported |
| boA9344-70cc | Feature not supported |
| boA9344-70cm | Feature not supported |
| boA13440-17cm | Feature not supported |
| daA720-520uc | Feature not supported |
| daA720-520um | Feature not supported |
| daA1280-54uc | Feature not supported |
| daA1280-54um | Feature not supported |
| daA1440-220uc | Feature not supported |
| daA1440-220um | Feature not supported |
| daA1600-60uc | Feature not supported |
| daA1600-60um | Feature not supported |
| daA1920-15um | Feature not supported |
| daA1920-30uc | Feature not supported |
| daA1920-30um | Feature not supported |
| daA1920-160uc | Feature not supported |
| daA1920-160um | Feature not supported |
| daA2448-70uc | Feature not supported |
| daA2448-70um | Feature not supported |
| daA2500-14uc | Feature not supported |
| daA2500-14um | Feature not supported |
| daA3840-45uc | Feature not supported |
| daA3840-45um | Feature not supported |
| dmA720-290gc | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| dmA720-290gm | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| dmA1440-73gc | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| dmA1440-73gm | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| dmA1920-51gc | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| dmA1920-51gm | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| dmA2048-37gc | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| dmA2048-37gm | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| dmA2448-23gc | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| dmA2448-23gm | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| dmA2840-14gc | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| dmA2840-14gm | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| dmA3536-9gc | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| dmA3536-9gm | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| dmA4096-9gc | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| dmA4096-9gm | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| puA1280-54uc | Feature not supported |
| puA1280-54um | Feature not supported |
| puA1600-60uc | Feature not supported |
| puA1600-60um | Feature not supported |
| puA1920-30uc | Feature not supported |
| puA1920-30um | Feature not supported |
| puA2500-14uc | Feature not supported |
| puA2500-14um | Feature not supported |
| r2L2048-29gc | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| r2L2048-58gm | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| r2L2048-62cc | Feature not supported |
| r2L2048-62g5c | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| r2L2048-172cm | Feature not supported |
| r2L2048-172g5m | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| r2L4096-14gc | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| r2L4096-29gm | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| r2L4096-42cc | Feature not supported |
| r2L4096-42g5c | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| r2L4096-84cm | Feature not supported |
| r2L4096-84g5m | BandwidthReserveMode BslDeviceLinkCurrentThroughput DeviceLinkThroughputLimit GevHeartbeatTimeout GevSCBWR GevSCBWRA GevSCFTD GevSCPD GevSCPSPacketSize PayloadSize |
| r2L8192-80cc | Feature not supported |
| r2L8192-240cm | Feature not supported |
| r2L16384-60cc | Feature not supported |
| r2L16384-120cm | Feature not supported |